#include < zll-types.h >

Data Fields

uint32_t bitmask
uint16_t freeNodeIdMin
uint16_t freeNodeIdMax
uint16_t myGroupIdMin
uint16_t freeGroupIdMin
uint16_t freeGroupIdMax
uint8_t rssiCorrection

Field Documentation

◆ bitmask

uint32_t EmberTokTypeStackZllData::bitmask

◆ freeGroupIdMax

uint16_t EmberTokTypeStackZllData::freeGroupIdMax

◆ freeGroupIdMin

uint16_t EmberTokTypeStackZllData::freeGroupIdMin

◆ freeNodeIdMax

uint16_t EmberTokTypeStackZllData::freeNodeIdMax

◆ freeNodeIdMin

uint16_t EmberTokTypeStackZllData::freeNodeIdMin

◆ myGroupIdMin

uint16_t EmberTokTypeStackZllData::myGroupIdMin

◆ rssiCorrection

uint8_t EmberTokTypeStackZllData::rssiCorrection

The documentation for this struct was generated from the following file:
  • zll-types.h