Bootloader GPIO definitions.
Enumerations |
|
| enum |
blState_e
{
BL_ST_UP , BL_ST_DOWN , BL_ST_POLLING_LOOP , BL_ST_DOWNLOAD_LOOP , BL_ST_DOWNLOAD_FAILURE , BL_ST_DOWNLOAD_SUCCESS } |
|
Defines various bootloader states. Use in LED code to signal bootload activity.
|
|
Functions |
|
| void | bootloadGpioInit (void) |
|
Initialize GPIO.
|
|
| void | bootloadStateIndicator (enum blState_e state) |
|
Helper function used for displaying bootloader state (for example: with LEDs).
|
|
| bool | bootloadForceActivation (void) |
|
Force activation of bootloader.
|
|
State Indicator Macros |
|
|
The bootloader indicates which state it is in by calling these // macros. Map them to the ::halBootloadStateIndicator function // (in bootloder-gpio.c) if you want to display that bootloader state. // Used to blink the LED's or otherwise signal bootloader activity. |
|
| #define | BL_STATE_UP () do { bootloadStateIndicator ( BL_ST_UP ); } while (0) |
|
Finished init sequence, ready for bootload.
|
|
| #define | BL_STATE_DOWN () do { bootloadStateIndicator ( BL_ST_DOWN ); } while (0) |
|
Called right before bootloader resets to application. Use to cleanup and reset GPIO's to leave node in known state for app start, if necessary.
|
|
| #define | BL_STATE_POLLING_LOOP () do { bootloadStateIndicator ( BL_ST_POLLING_LOOP ); } while (0) |
|
Standalone bootloader polling serial/radio interface.
|
|
| #define | BL_STATE_DOWNLOAD_LOOP () do { bootloadStateIndicator ( BL_ST_DOWNLOAD_LOOP ); } while (0) |
|
Processing download image.
|
|
| #define | BL_STATE_DOWNLOAD_SUCCESS () do { bootloadStateIndicator ( BL_ST_DOWNLOAD_SUCCESS ); } while (0) |
|
Download process was a success.
|
|
| #define | BL_STATE_DOWNLOAD_FAILURE () do { bootloadStateIndicator ( BL_ST_DOWNLOAD_FAILURE ); } while (0) |
|
Download process failed.
|
|
Detailed Description
Bootloader GPIO definitions.
See
bootloader-gpio.h
for source code.
Macro Definition Documentation
◆ BL_STATE_DOWN
| #define BL_STATE_DOWN | ( |
|
) | do { bootloadStateIndicator ( BL_ST_DOWN ); } while (0) |
Called right before bootloader resets to application. Use to cleanup and reset GPIO's to leave node in known state for app start, if necessary.
◆ BL_STATE_DOWNLOAD_FAILURE
| #define BL_STATE_DOWNLOAD_FAILURE | ( |
|
) | do { bootloadStateIndicator ( BL_ST_DOWNLOAD_FAILURE ); } while (0) |
Download process failed.
◆ BL_STATE_DOWNLOAD_LOOP
| #define BL_STATE_DOWNLOAD_LOOP | ( |
|
) | do { bootloadStateIndicator ( BL_ST_DOWNLOAD_LOOP ); } while (0) |
Processing download image.
◆ BL_STATE_DOWNLOAD_SUCCESS
| #define BL_STATE_DOWNLOAD_SUCCESS | ( |
|
) | do { bootloadStateIndicator ( BL_ST_DOWNLOAD_SUCCESS ); } while (0) |
Download process was a success.
◆ BL_STATE_POLLING_LOOP
| #define BL_STATE_POLLING_LOOP | ( |
|
) | do { bootloadStateIndicator ( BL_ST_POLLING_LOOP ); } while (0) |
Standalone bootloader polling serial/radio interface.
◆ BL_STATE_UP
| #define BL_STATE_UP | ( |
|
) | do { bootloadStateIndicator ( BL_ST_UP ); } while (0) |
Finished init sequence, ready for bootload.
Enumeration Type Documentation
◆ blState_e
| enum blState_e |
Function Documentation
◆ bootloadForceActivation()
| bool bootloadForceActivation | ( | void |
|
) |
Force activation of bootloader.
◆ bootloadGpioInit()
| void bootloadGpioInit | ( | void |
|
) |
Initialize GPIO.
◆ bootloadStateIndicator()
| void bootloadStateIndicator | ( | enum blState_e |
state
|
) |
Helper function used for displaying bootloader state (for example: with LEDs).