Configuration
User-configurable stack configuration macros and defaults. More...
         Macros | 
       |
| #define | EMBER_HEAP_SIZE 2000 | 
| 
         The size in bytes of the Ember heap. See
         
          Memory Buffer
         
         for more details.
         
          More...
         
          | 
       |
| #define | EMBER_CHILD_TABLE_SIZE 0 | 
| 
         The maximum number of children supported by the device. Can be configured from 0 to 64. 11B of token space is allocated for each child in the table.
         
          More...
         
          | 
       |
| #define | EMBER_CHILD_TABLE_TOKEN_SIZE EMBER_CHILD_TABLE_SIZE | 
| #define | EMBER_CHILD_TIMEOUT_SEC 3600 | 
| 
         Every child should exchange regularly some sort of traffic with the parent. Eventually, if traffic is not exchanged for a prolonged period of time, the parent may remove the child from the child table. In particular the parent shall remove the oldest stale child whenever the child table is full and there is the need of making room for a new child. Range extenders periodically exchange network-level commands with the coordinator. End devices and sleepy end devices can use
         
          emberPollForData()
         
         as keep alive mechanism, or use the
         
          Poll Plugin
         
         plugin. The maximum allowed timeout value is
         
          EMBER_CHILD_TABLE_MAX_TIMEOUT_S
         
         . Setting the timeout value to
         
          EMBER_CHILD_TABLE_AGING_DISABLED
         
         disables aging of the child table.
         
          More...
         
          | 
       |
| #define | EMBER_INDIRECT_QUEUE_SIZE 0 | 
| 
         Indirect queue is used on a parent to store a message intended for a sleepy end device, this configures the size of that queue. Configure it to 0 if parent support plugin is not used.
         
          More...
         
          | 
       |
| #define | EMBER_MAC_OUTGOING_QUEUE_SIZE 0 | 
| 
         MAC Outgoing paclet queue is to store messages until the radio is available to send it (In most cases, the radio is unavailable because it's already transmitting). The configures the size of that queue.
         
          More...
         
          | 
       |
| #define | EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS 8000 | 
| 
         The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child. The maximum value is 30 seconds (30000 milliseconds).
         
          More...
         
          | 
       |
| #define | EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC 60 | 
| 
         The period in seconds a range extender sends an update command to the coordinator containing the list of its children.
         
          More...
         
          | 
       |
| #define | EMBER_MAC_ACK_TIMEOUT_MS 25 | 
| 
         The ACK timeout in milliseconds. This parameter should be fine-tuned to reduce energy consumption for sleepy devices and depends on the data rate of the PHY configuration used. The maximum allowed value is 65.
         
          More...
         
          | 
       |
| #define | EMBER_RADIO_CCA_THRESHOLD -65 | 
| 
         The CCA threshold used at the MAC layer for CSMA/CA, in dBm.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_SEED 0 | 
| 
         The frequency hopping channel sequence generation seed. Can be configured between 0 and 65535. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_START_CHANNEL 0 | 
| 
         The lowest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_END_CHANNEL 24 | 
| 
         The highest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS 400 | 
| 
         The time in milliseconds to stay on each channel for frequency hopping. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS 20 | 
| 
         The time in milliseconds to guard each channel while frequency hopping. No MAC activity is allowed when entering or exiting the slot. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S 15 | 
| 
         The duration in seconds after which the server should broadcast its frequency hopping information to allow clients to realign. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_SLEEPY_CLIENT_RESYNC_PERIOD_S 60 | 
| 
         The duration in seconds after which a sleepy client should resync with the server if the last resync happened more than this duration ago. See the Frequency Hopping chapter of UG235.03 for more details.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_TIMEOUT_S (100) | 
         The maximum duration in seconds a non sleepy client would keep hopping without receiving frequency hopping information from the server, after which the synchronization with the server is deemed lost. A special value of
         
          EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_DISABLE_TIMEOUT
         
         disables this timeout.
         
          More...
         
          | 
       |
| #define | EMBER_FREQUENCY_HOPPING_SERVER_ADVERTISING_ITERATION_COUNT (3) | 
| 
         When a node is started a frequency hopping server, it will first advertise on all channels to resynchronize all existing clients in case the server was started as result of a reboot. This parameter defines the number of iterations over the entire hopping sequence.
         
          More...
         
          | 
       |
| #define | EMBER_COORDINATOR_FIRST_SHORT_ID_TO_BE_ASSIGNED 1 | 
| 
         An
         
          EMBER_STAR_COORDINATOR
         
         assigns short IDs to other nodes in the star network sequentially starting from this short ID. This option provides a simple effective way to reserve an pool of short addresses for commissioning.
         
          More...
         
          | 
       |
| #define | EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE 10 | 
| 
         The size of the short-to-long address mapping table. See
         
          emberMacAddShortToLongAddressMapping
         
         for more details.
         
          More...
         
          | 
       |
Detailed Description
User-configurable stack configuration macros and defaults.
Connect stack provides various interfaces to apply configuration:
- APIs to change configuration run-time
 - Manufacturing tokens to change configuration during device flashing
 - Macros to change configuration at compile-time
 
The compile time configuration macros and their default values are listed here.
The default values are always chosen to make it usable for most applications, but in some cases, you might need to change it. The recommended way is to either define the macro you need to change in the compilation command (e.g. gcc -D) or you by manipulating the configuration options in the configurator GUI.
      See
      
       ember-configuration-defaults.h
      
      for source code.
     
Macro Definition Documentation
◆ EMBER_CHILD_TABLE_SIZE
| #define EMBER_CHILD_TABLE_SIZE 0 | 
The maximum number of children supported by the device. Can be configured from 0 to 64. 11B of token space is allocated for each child in the table.
- Note
 - It's recommended to set it to 64 for EMBER_STAR_COORDINATOR , 32 for EMBER_STAR_RANGE_EXTENDER and 0 for anything else.
 
- Warning
 - This should be configured from the Parent Support plugin options.
 
        Definition at line
        
         102
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_CHILD_TABLE_TOKEN_SIZE
| #define EMBER_CHILD_TABLE_TOKEN_SIZE EMBER_CHILD_TABLE_SIZE | 
        Definition at line
        
         105
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_CHILD_TIMEOUT_SEC
| #define EMBER_CHILD_TIMEOUT_SEC 3600 | 
Every child should exchange regularly some sort of traffic with the parent. Eventually, if traffic is not exchanged for a prolonged period of time, the parent may remove the child from the child table. In particular the parent shall remove the oldest stale child whenever the child table is full and there is the need of making room for a new child. Range extenders periodically exchange network-level commands with the coordinator. End devices and sleepy end devices can use emberPollForData() as keep alive mechanism, or use the Poll Plugin plugin. The maximum allowed timeout value is EMBER_CHILD_TABLE_MAX_TIMEOUT_S . Setting the timeout value to EMBER_CHILD_TABLE_AGING_DISABLED disables aging of the child table.
- Warning
 - This should be configured from the Parent Support plugin options.
 
        Definition at line
        
         123
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_COORDINATOR_FIRST_SHORT_ID_TO_BE_ASSIGNED
| #define EMBER_COORDINATOR_FIRST_SHORT_ID_TO_BE_ASSIGNED 1 | 
An EMBER_STAR_COORDINATOR assigns short IDs to other nodes in the star network sequentially starting from this short ID. This option provides a simple effective way to reserve an pool of short addresses for commissioning.
        Definition at line
        
         276
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_TIMEOUT_S
| #define EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_TIMEOUT_S (100) | 
        The maximum duration in seconds a non sleepy client would keep hopping without receiving frequency hopping information from the server, after which the synchronization with the server is deemed lost. A special value of
        
         EMBER_FREQUENCY_HOPPING_ALWAYS_ON_CLIENT_SYNC_DISABLE_TIMEOUT
        
        disables this timeout.
       
        Definition at line
        
         256
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS
| #define EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS 400 | 
The time in milliseconds to stay on each channel for frequency hopping. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         218
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS
| #define EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS 20 | 
The time in milliseconds to guard each channel while frequency hopping. No MAC activity is allowed when entering or exiting the slot. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         227
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_END_CHANNEL
| #define EMBER_FREQUENCY_HOPPING_END_CHANNEL 24 | 
The highest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         210
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_SEED
| #define EMBER_FREQUENCY_HOPPING_SEED 0 | 
The frequency hopping channel sequence generation seed. Can be configured between 0 and 65535. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         194
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_SERVER_ADVERTISING_ITERATION_COUNT
| #define EMBER_FREQUENCY_HOPPING_SERVER_ADVERTISING_ITERATION_COUNT (3) | 
When a node is started a frequency hopping server, it will first advertise on all channels to resynchronize all existing clients in case the server was started as result of a reboot. This parameter defines the number of iterations over the entire hopping sequence.
        Definition at line
        
         266
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S
| #define EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S 15 | 
The duration in seconds after which the server should broadcast its frequency hopping information to allow clients to realign. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         236
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_SLEEPY_CLIENT_RESYNC_PERIOD_S
| #define EMBER_FREQUENCY_HOPPING_SLEEPY_CLIENT_RESYNC_PERIOD_S 60 | 
The duration in seconds after which a sleepy client should resync with the server if the last resync happened more than this duration ago. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         245
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_FREQUENCY_HOPPING_START_CHANNEL
| #define EMBER_FREQUENCY_HOPPING_START_CHANNEL 0 | 
The lowest channel on the frequency hopping list. See the Frequency Hopping chapter of UG235.03 for more details.
        Definition at line
        
         202
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_HEAP_SIZE
| #define EMBER_HEAP_SIZE 2000 | 
The size in bytes of the Ember heap. See Memory Buffer for more details.
- Warning
 - This should be configured from the Parent Support plugin options.
 
        Definition at line
        
         90
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_INDIRECT_QUEUE_SIZE
| #define EMBER_INDIRECT_QUEUE_SIZE 0 | 
Indirect queue is used on a parent to store a message intended for a sleepy end device, this configures the size of that queue. Configure it to 0 if parent support plugin is not used.
- Warning
 - This should be configured from the Parent Support plugin options.
 
        Definition at line
        
         139
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS
| #define EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS 8000 | 
The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child. The maximum value is 30 seconds (30000 milliseconds).
- Warning
 - This should be configured from the Parent Support plugin options.
 
        Definition at line
        
         159
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_MAC_ACK_TIMEOUT_MS
| #define EMBER_MAC_ACK_TIMEOUT_MS 25 | 
The ACK timeout in milliseconds. This parameter should be fine-tuned to reduce energy consumption for sleepy devices and depends on the data rate of the PHY configuration used. The maximum allowed value is 65.
        Definition at line
        
         177
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_MAC_OUTGOING_QUEUE_SIZE
| #define EMBER_MAC_OUTGOING_QUEUE_SIZE 0 | 
MAC Outgoing paclet queue is to store messages until the radio is available to send it (In most cases, the radio is unavailable because it's already transmitting). The configures the size of that queue.
- Warning
 - This should be configured from the MAC Packet Queue plugin options.
 
        Definition at line
        
         149
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC
| #define EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC 60 | 
The period in seconds a range extender sends an update command to the coordinator containing the list of its children.
- Attention
 - This option is only used on EMBER_STAR_RANGE_EXTENDER device.
 
        Definition at line
        
         168
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_RADIO_CCA_THRESHOLD
| #define EMBER_RADIO_CCA_THRESHOLD -65 | 
The CCA threshold used at the MAC layer for CSMA/CA, in dBm.
- Warning
 - This should be configured from the Connect Stack plugin options.
 
        Definition at line
        
         185
        
        of file
        
         ember-configuration-defaults.h
        
        .
       
◆ EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE
| #define EMBER_SECURITY_SHORT_TO_LONG_MAPPING_TABLE_SIZE 10 | 
The size of the short-to-long address mapping table. See emberMacAddShortToLongAddressMapping for more details.
- Attention
 - This table is only used for EMBER_MAC_MODE_DEVICE and EMBER_MAC_MODE_SLEEPY_DEVICE , but the memory will be allocated on all device types.
 
        Definition at line
        
         287
        
        of file
        
         ember-configuration-defaults.h
        
        .