Event Scheduling
Scheduling events for future execution. More...
         Macros | 
       |
| #define | __EVENT_H__ | 
| #define | EMBER_TASK_COUNT (3) | 
| 
         The number of event tasks that can be used to schedule and run events. Connect stack requires one, while another is used for Application Framework events.
         
          More...
         
          | 
       |
| #define | emberEventControlSetInactive (control) do { (control).status = EMBER_EVENT_INACTIVE ; } while (0) | 
| 
         Set this
         
          EmberEventControl
         
         as inactive (no pending event).
         
          More...
         
          | 
       |
| #define | emberEventControlGetActive (control) ((control).status != EMBER_EVENT_INACTIVE ) | 
| 
         Check whether this
         
          EmberEventControl
         
         is currently active. An event is considered active if it is set to run some time in the future (activated by
         
          emberEventControlSetActive()
         
         ,
         
          emberEventControlSetDelayMS()
         
         or any other emberEventControlSetDelay* functions)
         
          More...
         
          | 
       |
| #define | emberEventControlSetActive (control) do { emEventControlSetActive (&(control)); } while (0) | 
| 
         Set this
         
          EmberEventControl
         
         to run at the next available opportunity.
         
          More...
         
          | 
       |
| #define | EMBER_MAX_EVENT_CONTROL_DELAY_MS ( HALF_MAX_INT32U_VALUE - 1) | 
| 
         The maximum delay that may be passed to
         
          emberEventControlSetDelayMS()
         
         .
         
          More...
         
          | 
       |
| #define | emberEventControlSetDelayMS (control, delay) do { emEventControlSetDelayMS (&(control), (delay)); } while (0) | 
| 
         Set this
         
          EmberEventControl
         
         to run some milliseconds in the future.
         
          More...
         
          | 
       |
| #define | EMBER_MAX_EVENT_CONTROL_DELAY_QS ( EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 8) | 
| 
         The maximum delay that may be passed to
         
          emberEventControlSetDelayQS()
         
         .
         
          More...
         
          | 
       |
| #define | emberEventControlSetDelayQS (control, delay) do { emEventControlSetDelayMS (&(control), (delay) << 8); } while (0) | 
| 
         Set this
         
          EmberEventControl
         
         to run some quarter seconds in the future.
         
          More...
         
          | 
       |
| #define | EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES ( EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 16) | 
| 
         The maximum delay that may be passed to
         
          emberEventControlSetDelayMinutes()
         
         .
         
          More...
         
          | 
       |
| #define | emberEventControlSetDelayMinutes (control, delay) do { emEventControlSetDelayMS (&(control), (delay) << 16); } while (0) | 
| 
         Set this
         
          EmberEventControl
         
         to run some minutes in the future.
         
          More...
         
          | 
       |
| #define | emberEventControlGetRemainingMS (control) ( emEventControlGetRemainingMS (&(control))) | 
| 
         Check when the event is scheduled to run.
         
          More...
         
          | 
       |
| #define | emberTaskEnableIdling (allow) do { emTaskEnableIdling ((allow)); } while (0) | 
| 
         Enable or disable idling.
         
          More...
         
          | 
       |
| #define | emberMarkTaskActive (taskid) do { emMarkTaskActive ((taskid)); } while (0) | 
| 
         Calling it indicates that a task has something to do, so it should prevent the CPU from idling until
         
          emberMarkTaskIdle
         
         is next called on this task.
         
          More...
         
          | 
       |
         Functions | 
       |
| void | emEventControlSetActive ( EmberEventControl *event) | 
| void | emEventControlSetDelayMS ( EmberEventControl *event, uint32_t delay) | 
| uint32_t | emEventControlGetRemainingMS ( EmberEventControl *event) | 
| void | emberRunEvents ( EmberEventData *events) | 
| 
         Start an event handler if there is anything scheduled at the moment this function is called.
         
          More...
         
          | 
       |
| void | emberRunTask ( EmberTaskId taskid) | 
| 
         Start an event handler if there is anything scheduled at the moment this function is called.
         
          More...
         
          | 
       |
| uint32_t | emberMsToNextEvent ( EmberEventData *events, uint32_t maxMs) | 
| 
         Check when the next event is scheduled to run.
         
          More...
         
          | 
       |
| uint32_t | emberMsToNextEventExtended ( EmberEventData *events, uint32_t maxMs, uint8_t *returnIndex) | 
| uint32_t | emberMsToNextStackEvent (void) | 
| 
         Check when the next stack event is scheduled to run.
         
          More...
         
          | 
       |
| EmberTaskId | emberTaskInit ( EmberEventData *events) | 
| 
         Initialize a task for managing events and processor idling state.
         
          More...
         
          | 
       |
| bool | emberMarkTaskIdle ( EmberTaskId taskid) | 
| 
         Try to idle the CPU, unless any events in any tasks are pending.
         
          More...
         
          | 
       |
| void | emTaskEnableIdling (bool allow) | 
| 
         Enable or disable idling.
         
          More...
         
          | 
       |
| void | emMarkTaskActive ( EmberTaskId taskid) | 
| 
         Calling it indicates that a task has something to do, so it should prevent the CPU from idling until
         
          emberMarkTaskIdle
         
         is next called on this task.
         
          More...
         
          | 
       |
Detailed Description
Scheduling events for future execution.
See Event Scheduling for documentation. These macros implement an event abstraction that allows the application to schedule code to run after a specified time interval. An event consists of a procedure to be called at some point in the future and a control object that determines which procedure should be called. Events are also useful when an ISR needs to initiate an action that should run outside the ISR context.
      See
      
       event.h
      
      for source code.
     
Note that, while not required, it is recommended that the event-handling procedure explicitly define the recurrence of the next event, either by rescheduling via some kind of emberEventControlSetDelayXX() call or by deactivating via a call to emberEventControlSetInactive() .
When the handler does not explicitly reschedule or cancel the event, the default behavior of the event control system is to keep the event immediately active as if the handler function had called emberEventControlSetActive(someEvent) or emberEventControlSetDelayMS(someEvent, 0) .
The base time units for events are ticks. A tick equals 1us on every platform supported by Connect. Note, however, that the accuracy of the base tick depends on the timer source, which by default is the LF RC oscillator on EFR32 platforms.
Furthermore, the scheduled delay is the minimum delay. If emberRunEvents() or emberRunTask() are not called frequently enough, the actual delay may be longer than the scheduled delay.
Additionally, the APIs for quarter second and minute delays ( emberEventControlSetDelayQS() and emberEventControlSetDelayMinutes() ) use "binary" units. One quarter second is 256 ticks and one minute is 65536 ticks. These APIs are therefore doesn't actually mean a quarter of second or a minute on platforms supported by Connect.
However, in the future, Connect support might become available on platforms where one tick is not exactly 1us. For example,. on the EM357 SoC, 1ms is 1024 ticks, so each tick is 1000 / 1024 = ~0.98 milliseconds. If you need platform independent accurate delays, use the macros ::MILLISECOND_TICKS_PER_SECOND and ::MILLISECOND_TICKS_PER_MINUTE. For example, calling emberEventControlSetDelayMS(someEvent, 3 * MILLISECOND_TICKS_PER_MINUTE) will delay for 3 minutes on any platform.
The following are brief usage examples.
Macro Definition Documentation
◆ __EVENT_H__
| #define __EVENT_H__ | 
        Definition at line
        
         179
        
        of file
        
         event.h
        
        .
       
◆ EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES
| #define EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES ( EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 16) | 
The maximum delay that may be passed to emberEventControlSetDelayMinutes() .
        Definition at line
        
         272
        
        of file
        
         event.h
        
        .
       
◆ EMBER_MAX_EVENT_CONTROL_DELAY_MS
| #define EMBER_MAX_EVENT_CONTROL_DELAY_MS ( HALF_MAX_INT32U_VALUE - 1) | 
The maximum delay that may be passed to emberEventControlSetDelayMS() .
        Definition at line
        
         230
        
        of file
        
         event.h
        
        .
       
◆ EMBER_MAX_EVENT_CONTROL_DELAY_QS
| #define EMBER_MAX_EVENT_CONTROL_DELAY_QS ( EMBER_MAX_EVENT_CONTROL_DELAY_MS >> 8) | 
The maximum delay that may be passed to emberEventControlSetDelayQS() .
        Definition at line
        
         255
        
        of file
        
         event.h
        
        .
       
◆ EMBER_TASK_COUNT
| #define EMBER_TASK_COUNT (3) | 
The number of event tasks that can be used to schedule and run events. Connect stack requires one, while another is used for Application Framework events.
        Definition at line
        
         186
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlGetActive
| #define emberEventControlGetActive | ( | 
           
            control
           
           | 
          ) | ((control).status != EMBER_EVENT_INACTIVE ) | 
Check whether this EmberEventControl is currently active. An event is considered active if it is set to run some time in the future (activated by emberEventControlSetActive() , emberEventControlSetDelayMS() or any other emberEventControlSetDelay* functions)
- Parameters
 - 
         
[in] controlControl of the event in question.  
- Returns
 - Returns true if the event is active false otherwise
 
        Definition at line
        
         207
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlGetRemainingMS
| #define emberEventControlGetRemainingMS | ( | 
           
            control
           
           | 
          ) | ( emEventControlGetRemainingMS (&(control))) | 
Check when the event is scheduled to run.
- Parameters
 - 
         
[in] controlControl of the event in question.  
- Returns
 - Returns the amount of milliseconds remaining before the event is scheduled to run. If the event is inactive, MAX_INT32U_VALUE is returned.
 
        Definition at line
        
         291
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlSetActive
| #define emberEventControlSetActive | ( | 
           
            control
           
           | 
          ) | do { emEventControlSetActive (&(control)); } while (0) | 
Set this EmberEventControl to run at the next available opportunity.
- Parameters
 - 
         
[in] controlControl of the event to set active.  
        Definition at line
        
         216
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlSetDelayMinutes
| #define emberEventControlSetDelayMinutes | ( | 
           
            control,
           
           | 
         |
           
            delay
           
           | 
         |||
| ) | do { emEventControlSetDelayMS (&(control), (delay) << 16); } while (0) | 
Set this EmberEventControl to run some minutes in the future.
- Parameters
 - 
         
[in] controlControl of the event to run. [in] delayThe delay in minute. One minute is actually 65536 ms. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_MINUTES  
        Definition at line
        
         281
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlSetDelayMS
| #define emberEventControlSetDelayMS | ( | 
           
            control,
           
           | 
         |
           
            delay
           
           | 
         |||
| ) | do { emEventControlSetDelayMS (&(control), (delay)); } while (0) | 
Set this EmberEventControl to run some milliseconds in the future.
- Parameters
 - 
         
[in] controlControl of the event to run. [in] delayThe delay in milliseconds. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_MS  
        Definition at line
        
         239
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlSetDelayQS
| #define emberEventControlSetDelayQS | ( | 
           
            control,
           
           | 
         |
           
            delay
           
           | 
         |||
| ) | do { emEventControlSetDelayMS (&(control), (delay) << 8); } while (0) | 
Set this EmberEventControl to run some quarter seconds in the future.
- Parameters
 - 
         
[in] controlControl of the event to run. [in] delayThe delay in quarter seconds. One quarter second is actually 256 ms. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_QS  
- Warning
 - Applications should use emberEventControlSetDelayQS() instead.
 
        Definition at line
        
         266
        
        of file
        
         event.h
        
        .
       
◆ emberEventControlSetInactive
| #define emberEventControlSetInactive | ( | 
           
            control
           
           | 
          ) | do { (control).status = EMBER_EVENT_INACTIVE ; } while (0) | 
Set this EmberEventControl as inactive (no pending event).
- Parameters
 - 
         
[in] controlControl of the event to set inactive.  
        Definition at line
        
         193
        
        of file
        
         event.h
        
        .
       
◆ emberMarkTaskActive
| #define emberMarkTaskActive | ( | 
           
            taskid
           
           | 
          ) | do { emMarkTaskActive ((taskid)); } while (0) | 
Calling it indicates that a task has something to do, so it should prevent the CPU from idling until emberMarkTaskIdle is next called on this task.
- Parameters
 - 
         
[in] taskidThe task to mark active.  
        Definition at line
        
         417
        
        of file
        
         event.h
        
        .
       
◆ emberTaskEnableIdling
| #define emberTaskEnableIdling | ( | 
           
            allow
           
           | 
          ) | do { emTaskEnableIdling ((allow)); } while (0) | 
Enable or disable idling.
- Parameters
 - 
         
[in] allowSetting it to true will enable, while setting it to false will disable idling.  
        Definition at line
        
         402
        
        of file
        
         event.h
        
        .
       
Function Documentation
◆ emberMarkTaskIdle()
| bool emberMarkTaskIdle | ( | EmberTaskId | 
           
            taskid
           
           | 
          ) | 
Try to idle the CPU, unless any events in any tasks are pending.
- Parameters
 - 
         
[in] taskidthe task which should handle the idling.  
- Returns
 - Returns true if the processor was idled false if idling wasn't permitted because a task has something to do.
 
- Note
 - This API should always be called with interrupts disabled. It will forcibly re-enable interrupts before returning.
 
◆ emberMsToNextEvent()
| uint32_t emberMsToNextEvent | ( | EmberEventData * | 
           
            events,
           
           | 
         
| uint32_t | 
           
            maxMs
           
           | 
         ||
| ) | 
Check when the next event is scheduled to run.
- Parameters
 - 
         
[in] eventsAn array of events to check. [in] maxMsIf no event is scheduled before maxMs, maxMs will be returned  
- Returns
 - 
         Returns the number of milliseconds before the next event is scheduled to expire, or
         
maxMsif no event is scheduled to expire within that time. 
- Note
 - If any events are modified within an interrupt, to guarantee the accuracy of this API, it must be called with interrupts disabled.
 
- See also
 - emberMsToNextEventExtended()
 
◆ emberMsToNextEventExtended()
| uint32_t emberMsToNextEventExtended | ( | EmberEventData * | 
           
            events,
           
           | 
         
| uint32_t | 
           
            maxMs,
           
           | 
         ||
| uint8_t * | 
           
            returnIndex
           
           | 
         ||
| ) | 
Check when the next event is scheduled to run.
- Parameters
 - 
         
[in] eventsAn array of events to check. [in] maxMsIf no event is scheduled before maxMs, maxMs will be returned [out] returnIndexIf not NULL pointer was passed, the index of the next event will be returned here, or 0xFF if no event is scheduled before maxMs.  
- Returns
 - 
         Returns the number of milliseconds before the next event is scheduled to expire, or
         
maxMsif no event is scheduled to expire within that time. 
- Note
 - If any events are modified within an interrupt, to guarantee the accuracy of this API, it must be called with interrupts disabled.
 
- See also
 - emberMsToNextEvent()
 
◆ emberMsToNextStackEvent()
| uint32_t emberMsToNextStackEvent | ( | void | 
           
           
           | 
          ) | 
Check when the next stack event is scheduled to run.
- Returns
 - Returns the number of milliseconds before the next stack event is scheduled to run.
 
◆ emberRunEvents()
| void emberRunEvents | ( | EmberEventData * | 
           
            events
           
           | 
          ) | 
Start an event handler if there is anything scheduled at the moment this function is called.
An application typically creates an array of events along with their handlers. This function should be called in the main loop to run those events.
- Parameters
 - 
         
[in] eventsPointer to the array of events.  
- Warning
 - This is normally handled by emberRunTask() in the main plugin.
 
◆ emberRunTask()
| void emberRunTask | ( | EmberTaskId | 
           
            taskid
           
           | 
          ) | 
Start an event handler if there is anything scheduled at the moment this function is called.
If an application has initialized a task via emberTaskInit() , to run the events associated with that task, it should call emberRunTask() instead of emberRunEvents() .
- Warning
 - This is normally handled by the main plugin.
 
◆ emberTaskInit()
| EmberTaskId emberTaskInit | ( | EmberEventData * | 
           
            events
           
           | 
          ) | 
Initialize a task for managing events and processor idling state.
- Parameters
 - 
         
[in] eventsPointer to the array of events to manage  
- Returns
 - Returns the EmberTaskId which represents the newly created task.
 
- Note
 - After the task is created emberRunTask() should be called periodically.
 
◆ emEventControlGetRemainingMS()
| uint32_t emEventControlGetRemainingMS | ( | EmberEventControl * | 
           
            event
           
           | 
          ) | 
Check when the event is scheduled to run.
- Parameters
 - 
         
[in] eventPointer to the control of the event in question.  
- Returns
 - Return the amount of milliseconds remaining before the event is scheduled to run. If the event is inactive, MAX_INT32U_VALUE is returned.
 
- Warning
 - Applications should use emberEventControlGetRemainingMS() instead.
 
◆ emEventControlSetActive()
| void emEventControlSetActive | ( | EmberEventControl * | 
           
            event
           
           | 
          ) | 
Set this EmberEventControl to run at the next available opportunity.
- Parameters
 - 
         
[in] eventPointer to the control of the event to set active  
- Warning
 - Applications should use emberEventControlSetActive() instead.
 
◆ emEventControlSetDelayMS()
| void emEventControlSetDelayMS | ( | EmberEventControl * | 
           
            event,
           
           | 
         
| uint32_t | 
           
            delay
           
           | 
         ||
| ) | 
Set this EmberEventControl to run some milliseconds in the future.
- Parameters
 - 
         
[in] eventPointer to the control of the event to run. [in] delayThe delay in milliseconds. Must be less than EMBER_MAX_EVENT_CONTROL_DELAY_MS  
- Warning
 - Applications should use emberEventControlSetDelayMS() instead.
 
◆ emMarkTaskActive()
| void emMarkTaskActive | ( | EmberTaskId | 
           
            taskid
           
           | 
          ) | 
Calling it indicates that a task has something to do, so it should prevent the CPU from idling until emberMarkTaskIdle is next called on this task.
- Parameters
 - 
         
[in] taskidThe task to mark active.  
- Warning
 - Applications should use emberMarkTaskActive() instead.
 
◆ emTaskEnableIdling()
| void emTaskEnableIdling | ( | bool | 
           
            allow
           
           | 
          ) | 
Enable or disable idling.
- Parameters
 - 
         
[in] allowSetting it to true will enable, while setting it to false will disable idling.  
- Warning
 - Applications should use emberTaskEnableIdling() instead.