EmberMacAddress Struct Reference
A structure that stores an 802.15.4 address. More...
      
       #include <
       
     
        ember-types.h
       
       >
      
         Data Fields | 
       |
| union { | |
| uint8_t longAddress [ EUI64_SIZE ] | |
         Long (EUI-64) address. Valid if
         
          mode
         
         is
         
          EMBER_MAC_ADDRESS_MODE_LONG
         
         .
         
          More...
         
          | 
       |
| uint16_t shortAddress | |
         Short address (node ID). Valid if
         
          mode
         
         is
         
          EMBER_MAC_ADDRESS_MODE_SHORT
         
         .
         
          More...
         
          | 
       |
| } | addr | 
| EmberMacAddressMode | mode | 
A structure that stores an 802.15.4 address.
       Definition at line
       
        351
       
       of file
       
        ember-types.h
       
       .
      
Field Documentation
◆ addr
| union { ... } EmberMacAddress::addr | 
◆ longAddress
| uint8_t EmberMacAddress::longAddress[ EUI64_SIZE ] | 
        Long (EUI-64) address. Valid if
        
         mode
        
        is
        
         EMBER_MAC_ADDRESS_MODE_LONG
        
        .
       
        Definition at line
        
         357
        
        of file
        
         ember-types.h
        
        .
       
◆ mode
| EmberMacAddressMode EmberMacAddress::mode | 
Addressing mode
        Definition at line
        
         365
        
        of file
        
         ember-types.h
        
        .
       
◆ shortAddress
| uint16_t EmberMacAddress::shortAddress | 
        Short address (node ID). Valid if
        
         mode
        
        is
        
         EMBER_MAC_ADDRESS_MODE_SHORT
        
        .
       
        Definition at line
        
         362
        
        of file
        
         ember-types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
ember-types.h