Sample API funtions for controlling LEDs. More...
         Typedefs | 
       |
| typedef enum HalBoardLedPins | HalBoardLed | 
| 
         Ensures that the definitions from the BOARD_HEADER are always used as parameters to the LED functions.
         
          More...
         
          | 
       |
         Functions | 
       |
| void | halInternalInitLed (void) | 
| 
         Configures GPIOs pertaining to the control of LEDs.
         
          More...
         
          | 
       |
| void | halToggleLed ( HalBoardLed led) | 
| 
         Atomically wraps an XOR or similar operation for a single GPIO pin attached to an LED.
         
          More...
         
          | 
       |
| void | halSetLed ( HalBoardLed led) | 
| 
         Turns on (sets) a GPIO pin connected to an LED so that the LED turns on.
         
          More...
         
          | 
       |
| void | halClearLed ( HalBoardLed led) | 
| 
         Turns off (clears) a GPIO pin connected to an LED, which turns off the LED.
         
          More...
         
          | 
       |
| void | halStackIndicateActivity (bool turnOn) | 
         Called by the stack to indicate activity over the radio (for both transmission and reception). It is called once with
         
          turnOn
         
         true and shortly thereafter with
         
          turnOn
         
         false.
         
          More...
         
          | 
       |
Detailed Description
Sample API funtions for controlling LEDs.
When specifying an LED to use, always use the BOARDLEDx definitions that are defined within the BOARD_HEADER.
      See
      
       led.h
      
      for source code.
     
Typedef Documentation
◆ HalBoardLed
| typedef enum HalBoardLedPins HalBoardLed | 
Ensures that the definitions from the BOARD_HEADER are always used as parameters to the LED functions.
        Definition at line
        
         78
        
        of file
        
         led.h
        
        .
       
Function Documentation
◆ halClearLed()
| void halClearLed | ( | HalBoardLed | 
           
            led
           
           | 
          ) | 
Turns off (clears) a GPIO pin connected to an LED, which turns off the LED.
- Parameters
 - 
         
ledIdentifier (from BOARD_HEADER) for the LED to turn off.  
◆ halInternalInitLed()
| void halInternalInitLed | ( | void | 
           
           
           | 
          ) | 
Configures GPIOs pertaining to the control of LEDs.
◆ halSetLed()
| void halSetLed | ( | HalBoardLed | 
           
            led
           
           | 
          ) | 
Turns on (sets) a GPIO pin connected to an LED so that the LED turns on.
- Parameters
 - 
         
ledIdentifier (from BOARD_HEADER) for the LED to turn on.  
◆ halStackIndicateActivity()
| void halStackIndicateActivity | ( | bool | 
           
            turnOn
           
           | 
          ) | 
        Called by the stack to indicate activity over the radio (for both transmission and reception). It is called once with
        
         turnOn
        
        true and shortly thereafter with
        
         turnOn
        
        false.
       
Typically does something interesting, such as change the state of an LED.
- Parameters
 - 
         
turnOnSee Usage.  
◆ halToggleLed()
| void halToggleLed | ( | HalBoardLed | 
           
            led
           
           | 
          ) | 
Atomically wraps an XOR or similar operation for a single GPIO pin attached to an LED.
- Parameters
 - 
         
ledIdentifier (from BOARD_HEADER) for the LED to be toggled.