Stack Counters
Stack counters API. More...
         Functions | 
       |
| EmberStatus | emberGetCounter ( EmberCounterType counterType, uint32_t *count) | 
| 
         Retrieve the stack counter corresponding to the passed counter type.
         
          More...
         
          | 
       |
Detailed Description
Stack counters API.
Function Documentation
◆ emberGetCounter()
| EmberStatus emberGetCounter | ( | EmberCounterType | 
           
            counterType,
           
           | 
         
| uint32_t * | 
           
            count
           
           | 
         ||
| ) | 
Retrieve the stack counter corresponding to the passed counter type.
- Parameters
 - 
         
[in] counterTypeAn EmberCounterType value indicating the stack counter to be retrieved. [out] countThe counter of the requested counterTypeis returned here 
- Returns
 - An EmberStatus value of EMBER_SUCCESS if the stack counter was successfully retrieved. An EmberStatus value of EMBER_INVALID_CALL if the passed counterType is invalid. An EmberStatus value of EMBER_LIBRARY_NOT_PRESENT if the stack counter library is not present.