tokTypeStackNodeData Struct Reference
Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token. More...
      
       #include <
       
     
        token-stack.h
       
       >
      
         Data Fields | 
       |
| uint16_t | panId | 
| int16_t | radioTxPower | 
| uint16_t | radioFreqChannel | 
| uint8_t | nodeType | 
| uint16_t | nodeId | 
| uint16_t | parentId | 
Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token.
       Definition at line
       
        244
       
       of file
       
        token-stack.h
       
       .
      
Field Documentation
◆ nodeId
| uint16_t tokTypeStackNodeData::nodeId | 
The NodeId (short address) of the device
        Definition at line
        
         249
        
        of file
        
         token-stack.h
        
        .
       
◆ nodeType
| uint8_t tokTypeStackNodeData::nodeType | 
The EmberNodeType configured for the device
        Definition at line
        
         248
        
        of file
        
         token-stack.h
        
        .
       
◆ panId
| uint16_t tokTypeStackNodeData::panId | 
The PanId of the device
        Definition at line
        
         245
        
        of file
        
         token-stack.h
        
        .
       
◆ parentId
| uint16_t tokTypeStackNodeData::parentId | 
The NodeId of the device's parent, if any
        Definition at line
        
         250
        
        of file
        
         token-stack.h
        
        .
       
◆ radioFreqChannel
| uint16_t tokTypeStackNodeData::radioFreqChannel | 
The radio channel configured for the device
        Definition at line
        
         247
        
        of file
        
         token-stack.h
        
        .
       
◆ radioTxPower
| int16_t tokTypeStackNodeData::radioTxPower | 
The TX power configured for the device in deci-dBm
        Definition at line
        
         246
        
        of file
        
         token-stack.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
token-stack.h