Connect Stack Native API
Here is a list of all modules:
| Connect Stack API Reference | The primary API towards the Connect radio stack |
| Connect Stack Version | Macros to determine the stack version |
| Connect Data Types | Definitions of Connect data types used by various Connect API functions |
| Stack Information | Connect API for accessing and modifying stack states and behaviors |
| Stack Counters | Stack counters API |
| Network Management | Connect API for finding, forming, joining, and leaving Connect networks |
| Frequency Hopping | API and callbacks for frequency hopping configuration |
| Parent Support | |
| Radio Stream | Radio stream API |
| Configuration | User-configurable stack configuration macros and defaults |
| Status Codes | Return-code definitions for Connect stack API functions |
| Stack Tokens | Definitions for stack tokens |
| Event Scheduling | Scheduling events for future execution |
| Memory Buffer | Ember Connect API dynamically allocates and frees memory |
| Messaging | Connect APIs and handlers for sending and receiving messages |
| Connect Application Framework API Reference | Application Framework includes plugins that are built on top of the Connect stack |
| Application Framework Common | Application framework common |
| Command Interpreter Plugin | Processes commands coming from the serial port |
| Debug Print Plugin | |
| Mailbox Client Plugin | APIs for mailbox client |
| Mailbox Server Plugin | APIs for mailbox server |
| Mailbox Common | Types defined for mailbox |
| Ota Unicast Bootloader Client Plugin | APIs/callbacks for ota-unicast-bootloader clients |
| Ota Unicast Bootloader Server Plugin | Macros and APIs for ota-unicast-bootloader server |
| Ota Unicast Bootloader Common | Macros and types defined for ota-unicast-bootloaders |
| Ota Broadcast Bootloader Client Plugin | Set of APIs for ota-broadcast-bootloader-client |
| Ota Broadcast Bootloader Server Plugin | Set of APIs for ota-broadcast-bootloader-server |
| Ota Broadcast Bootloader Common | Set of types defined for ota-broadcast-bootloader |
| Poll Plugin | APIs for the poll plugin |
| WSTK Sensors Plugin | |
| Hardware Abstraction Layer (HAL) API Reference | |
| Common Microcontroller Functions | |
| Token Access | |
| Tokens | |
| Simulated EEPROM | |
| Sample APIs for Peripheral Access | |
| Serial UART Communication | This API contains the HAL interfaces that applications must implement for the high-level serial code |
| Button Control | Sample API functions for using push-buttons |
| Buzzer Control | |
| LED Control | Sample API funtions for controlling LEDs |
| Flash Memory Control | Definition and description of public flash manipulation routines |
| System Timer Control | Functions that provide access to the system clock |
| Symbol Timer Control | |
| HAL Configuration | |
| Sample Breakout Board Configuration | |
| IAR PLATFORM_HEADER Configuration | Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler |
| Common PLATFORM_HEADER Configuration | Compiler and Platform specific definitions and typedefs common to all platforms |
| NVIC Configuration | |
| Reset Cause Type Definitions | |
| HAL Utilities | |
| Crash and Watchdog Diagnostics | Crash and watchdog diagnostic functions |
| Cyclic Redundancy Code (CRC) |
Functions that provide access to cyclic redundancy code (CRC) calculation. See
crc.h
for source code
|
| Random Number Generation | Functions that provide access to random numbers |
| Network to Host Byte Order Conversion |