EmberIncomingMessage Struct Reference
An instance of this structure is passed to emberIncomingMessageHandler() . It describes the incoming message. More...
      
       #include <
       
     
        ember-types.h
       
       >
      
         Data Fields | 
       |
| EmberMessageOptions | options | 
| EmberNodeId | source | 
| uint8_t | endpoint | 
| int8_t | rssi | 
| EmberMessageLength | length | 
| uint8_t * | payload | 
| uint32_t | timestamp | 
| uint8_t | lqi | 
An instance of this structure is passed to emberIncomingMessageHandler() . It describes the incoming message.
       Definition at line
       
        247
       
       of file
       
        ember-types.h
       
       .
      
Field Documentation
◆ endpoint
| uint8_t EmberIncomingMessage::endpoint | 
The endpoint the message is destined to.
        Definition at line
        
         260
        
        of file
        
         ember-types.h
        
        .
       
◆ length
| EmberMessageLength EmberIncomingMessage::length | 
An EmberMessageLength value indicating the length in bytes of the incoming message.
        Definition at line
        
         269
        
        of file
        
         ember-types.h
        
        .
       
◆ lqi
| uint8_t EmberIncomingMessage::lqi | 
The LQI the packet was received with.
        Definition at line
        
         282
        
        of file
        
         ember-types.h
        
        .
       
◆ options
| EmberMessageOptions EmberIncomingMessage::options | 
An EmberMessageOptions value indicating the options used for the incoming packet.
        Definition at line
        
         252
        
        of file
        
         ember-types.h
        
        .
       
◆ payload
| uint8_t* EmberIncomingMessage::payload | 
A pointer to the message payload.
        Definition at line
        
         273
        
        of file
        
         ember-types.h
        
        .
       
◆ rssi
| int8_t EmberIncomingMessage::rssi | 
The RSSI in dBm the packet was received with.
        Definition at line
        
         264
        
        of file
        
         ember-types.h
        
        .
       
◆ source
| EmberNodeId EmberIncomingMessage::source | 
An EmberNodeId value indicating source node ID.
        Definition at line
        
         256
        
        of file
        
         ember-types.h
        
        .
       
◆ timestamp
| uint32_t EmberIncomingMessage::timestamp | 
The millisecond system time returned by halCommonGetInt32uMillisecondTick() at the time the sync word was detected.
        Definition at line
        
         278
        
        of file
        
         ember-types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
ember-types.h