Radio Stream
Radio stream API. More...
Functions |
|
| EmberStatus | emberStartTxStream ( EmberTxStreamParameters parameters, uint16_t channel) |
|
Start a continuous Tx stream to test RF.
More...
|
|
| EmberStatus | emberStopTxStream (void) |
|
Stop a RF stream in progress.
More...
|
|
Detailed Description
Radio stream API.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
Connect API managing radio stream for RF testing purpose
See
radio-stream.h
for source code.
Function Documentation
◆ emberStartTxStream()
| EmberStatus emberStartTxStream | ( | EmberTxStreamParameters |
parameters,
|
| uint16_t |
channel
|
||
| ) |
Start a continuous Tx stream to test RF.
- Parameters
-
[in] parametersStream mode. See EmberTxStreamParameters . [in] channelRF channel.
- Returns
-
EMBER_INVALID_CALL if the stack can not process the request
EMBER_BAD_ARGUMENT if the parameters are wrong
EMBER_SUCCESS if the stream can be started
◆ emberStopTxStream()
| EmberStatus emberStopTxStream | ( | void |
|
) |
Stop a RF stream in progress.
- Returns
-
EMBER_INVALID_CALL if no stream is in progress
EMBER_SUCCESS otherwise