Connect Data Types
Definitions of Connect data types used by various Connect API functions. More...
         Data Structures | 
       |
| struct | EmberNetworkParameters | 
| 
         Hold network parameters.
         
          More...
         
          | 
       |
| struct | EmberIncomingMessage | 
| 
         An instance of this structure is passed to
         
          emberIncomingMessageHandler()
         
         . It describes the incoming message.
         
          More...
         
          | 
       |
| struct | EmberOutgoingMessage | 
| 
         An instance of this structure is passed to
         
          emberMessageSentHandler()
         
         . It describes the outgoing packet.
         
          More...
         
          | 
       |
| struct | EmberMacAddress | 
| 
         A structure that stores an 802.15.4 address.
         
          More...
         
          | 
       |
| struct | EmberMacFrame | 
| 
         A structure that describes the addressing fields of a 802.15.4 frame.
         
          More...
         
          | 
       |
| struct | EmberIncomingMacMessage | 
| 
         An instance of this structure is passed to
         
          emberIncomingMacMessageHandler()
         
         . It describes the incoming MAC frame.
         
          More...
         
          | 
       |
| struct | EmberOutgoingMacMessage | 
| 
         An instance of this structure is passed to
         
          emberMacMessageSentHandler()
         
         . It describes the outgoing MAC frame.
         
          More...
         
          | 
       |
| struct | EmberKeyData | 
| 
         This data structure contains the security key, most prominently used by
         
          emberSetSecurityKey
         
         .
         
          More...
         
          | 
       |
| struct | EventActions | 
| 
         The static part of an event. Each event can be used with only one event queue.
         
          More...
         
          | 
       |
| struct | Event_s | 
| struct | EventQueue_s | 
| 
         An event queue is currently just a list of events ordered by execution time.
         
          More...
         
          | 
       |
| struct | EmberEventControl | 
| 
         Control structure for events.
         
          More...
         
          | 
       |
| struct | EmberEventData_S | 
| 
         Complete events with a control and a handler procedure.
         
          More...
         
          | 
       |
| struct | EmberTaskControl | 
| 
         Control structure for tasks.
         
          More...
         
          | 
       |
         Macros | 
       |
| #define | EXTENDED_PAN_ID_SIZE 8 | 
| 
         Size of an extended PAN identifier in bytes (8).
         
          More...
         
          | 
       |
| #define | EUI64_SIZE 8 | 
| 
         Size of EUI64 (an IEEE address) in bytes (8).
         
          More...
         
          | 
       |
| #define | EMBER_ENCRYPTION_KEY_SIZE 16 | 
| 
         Size of an encryption key in bytes (16).
         
          More...
         
          | 
       |
| #define | EMBER_NULL_NODE_ID 0xFFFFu | 
| 
         A distinguished network ID that will never be assigned to any node. Used to indicate the absence of a node ID.
         
          More...
         
          | 
       |
| #define | EMBER_BROADCAST_ADDRESS 0xFFFF | 
| 
         Broadcast address.
         
          More...
         
          | 
       |
| #define | EMBER_USE_LONG_ADDRESS 0xFFFE | 
| 
         Special short address indicating the node should use long addressing as source address.
         
          More...
         
          | 
       |
| #define | EMBER_COORDINATOR_ADDRESS 0x0000 | 
| 
         The coordinator short address.
         
          More...
         
          | 
       |
| #define | EMBER_CAL_INVALID_VALUE (0xFFFFFFFF) | 
         Typedefs | 
       |
| typedef uint8_t | EmberEUI64 [ EUI64_SIZE ] | 
| 
         EUI 64-bit ID (IEEE 802.15.4 long address).
         
          More...
         
          | 
       |
| typedef uint16_t | EmberNodeId | 
| 
         IEEE 802.15.4 node ID. Also known as short address.
         
          More...
         
          | 
       |
| typedef uint16_t | EmberPanId | 
| 
         IEEE 802.15.4 PAN ID.
         
          More...
         
          | 
       |
| typedef uint8_t | EmberMessageLength | 
| 
         Message length in bytes.
         
          More...
         
          | 
       |
| typedef uint8_t | EmberTaskId | 
| 
         An identifier for a task.
         
          More...
         
          | 
       |
| typedef struct Event_s | Event | 
| typedef struct EventQueue_s | EventQueue | 
| 
         An event queue is currently just a list of events ordered by execution time.
         
          More...
         
          | 
       |
| typedef PGM struct EmberEventData_S | EmberEventData | 
| typedef uint16_t | EmberBuffer | 
| 
         Buffers used by the memory buffer system.
         
          More...
         
          | 
       |
         Functions | 
       |
| uint8_t * | emberKeyContents ( EmberKeyData *key) | 
| 
         This macro allows the programmer to gain access to the key data bytes of the
         
          EmberKeyData
         
         structure.
         
          More...
         
          | 
       |
Detailed Description
Definitions of Connect data types used by various Connect API functions.
      See
      
       ember-types.h
      
      for source code.
     
Macro Definition Documentation
◆ EMBER_BROADCAST_ADDRESS
| #define EMBER_BROADCAST_ADDRESS 0xFFFF | 
Broadcast address.
        Definition at line
        
         88
        
        of file
        
         ember-types.h
        
        .
       
◆ EMBER_CAL_INVALID_VALUE
| #define EMBER_CAL_INVALID_VALUE (0xFFFFFFFF) | 
        Definition at line
        
         800
        
        of file
        
         ember-types.h
        
        .
       
◆ EMBER_COORDINATOR_ADDRESS
| #define EMBER_COORDINATOR_ADDRESS 0x0000 | 
The coordinator short address.
        Definition at line
        
         95
        
        of file
        
         ember-types.h
        
        .
       
◆ EMBER_ENCRYPTION_KEY_SIZE
| #define EMBER_ENCRYPTION_KEY_SIZE 16 | 
Size of an encryption key in bytes (16).
        Definition at line
        
         64
        
        of file
        
         ember-types.h
        
        .
       
◆ EMBER_NULL_NODE_ID
| #define EMBER_NULL_NODE_ID 0xFFFFu | 
A distinguished network ID that will never be assigned to any node. Used to indicate the absence of a node ID.
        Definition at line
        
         85
        
        of file
        
         ember-types.h
        
        .
       
◆ EMBER_USE_LONG_ADDRESS
| #define EMBER_USE_LONG_ADDRESS 0xFFFE | 
Special short address indicating the node should use long addressing as source address.
        Definition at line
        
         92
        
        of file
        
         ember-types.h
        
        .
       
◆ EUI64_SIZE
| #define EUI64_SIZE 8 | 
Size of EUI64 (an IEEE address) in bytes (8).
        Definition at line
        
         59
        
        of file
        
         ember-types.h
        
        .
       
◆ EXTENDED_PAN_ID_SIZE
| #define EXTENDED_PAN_ID_SIZE 8 | 
Size of an extended PAN identifier in bytes (8).
        Definition at line
        
         54
        
        of file
        
         ember-types.h
        
        .
       
Typedef Documentation
◆ EmberBuffer
| typedef uint16_t EmberBuffer | 
Buffers used by the memory buffer system.
        Definition at line
        
         755
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberEUI64
| typedef uint8_t EmberEUI64[ EUI64_SIZE ] | 
EUI 64-bit ID (IEEE 802.15.4 long address).
        Definition at line
        
         69
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberEventData
| typedef PGM struct EmberEventData_S EmberEventData | 
◆ EmberMessageLength
| typedef uint8_t EmberMessageLength | 
Message length in bytes.
        Definition at line
        
         215
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberNodeId
| typedef uint16_t EmberNodeId | 
IEEE 802.15.4 node ID. Also known as short address.
        Definition at line
        
         74
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberPanId
| typedef uint16_t EmberPanId | 
IEEE 802.15.4 PAN ID.
        Definition at line
        
         79
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberTaskId
| typedef uint8_t EmberTaskId | 
An identifier for a task.
        Definition at line
        
         536
        
        of file
        
         ember-types.h
        
        .
       
◆ Event
◆ EventQueue
| typedef struct EventQueue_s EventQueue | 
An event queue is currently just a list of events ordered by execution time.
Enumeration Type Documentation
◆ anonymous enum
| anonymous enum | 
Define tasks that prevent the stack from sleeping.
| Enumerator | |
|---|---|
| EMBER_OUTGOING_MESSAGES | 
            Messages are waiting for transmission.  | 
         
| EMBER_INCOMING_MESSAGES | 
            One or more incoming messages are processed.  | 
         
| EMBER_RADIO_IS_ON | 
            The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices, i.e., EMBER_STAR_COORDINATOR , EMBER_STAR_RANGE_EXTENDER , EMBER_STAR_END_DEVICE , or EMBER_MAC_MODE_DEVICE , the radio is always on.  | 
         
| EMBER_ASSOCIATING | 
            The node is currently trying to associate to a Connect network.  | 
         
| EMBER_SCANNING | 
            The node is currently performing a MAC-level scanning procedure.  | 
         
        Definition at line
        
         619
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberCalType
| enum EmberCalType | 
◆ EmberChildFlags
| enum EmberChildFlags | 
Child flags.
        Definition at line
        
         194
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberCounterType
| enum EmberCounterType | 
Define the event counters that can be requested from the application using emberGetCounter()
        Definition at line
        
         642
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberEventUnits
| enum EmberEventUnits | 
Either marks an event as inactive or specifies the units for the event execution time.
        Definition at line
        
         517
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberMacAddressMode
| enum EmberMacAddressMode | 
◆ EmberMessageOptions
| enum EmberMessageOptions | 
Message options.
| Enumerator | |
|---|---|
| EMBER_OPTIONS_NONE | 
            No options.  | 
         
| EMBER_OPTIONS_SECURITY_ENABLED | 
            The packet should be sent out encrypted.  | 
         
| EMBER_OPTIONS_ACK_REQUESTED | 
            An acknowledgment should be requested for the outgoing packet.  | 
         
| EMBER_OPTIONS_HIGH_PRIORITY | 
            The packet should be sent with high priority. High priority messages are added to the head of transmit queue, other messages are added to the tail.  | 
         
| EMBER_OPTIONS_INDIRECT | 
            The packet should be sent via the indirect queue. This option only applies to nodes with EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE node type.  | 
         
        Definition at line
        
         221
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberNetworkStatus
| enum EmberNetworkStatus | 
Defines the possible join states for a node.
        Definition at line
        
         158
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberNodeType
| enum EmberNodeType | 
Define the possible types of nodes and the roles that a node might play in a network.
| Enumerator | |
|---|---|
| EMBER_UNKNOWN_DEVICE | 
            Device is not in network.  | 
         
| EMBER_STAR_COORDINATOR | 
            Extended star mode device: Will relay messages and can act as a parent to range extender and end device nodes. A node can be started as a coordinator using the emberFormNetwork() API.  | 
         
| EMBER_STAR_RANGE_EXTENDER | 
            Extended star mode device: Will relay messages and can act as a parent to end device nodes. Joins to a coordinator. A node can be started as a range extender using the emberJoinNetwork() or emberJoinNetworkExtended() API.  | 
         
| EMBER_STAR_END_DEVICE | 
            Extended star mode device: Communicates only with its parent and will not relay messages. A node can be started as an end device using the emberJoinNetwork() or emberJoinNetworkExtended() API.  | 
         
| EMBER_STAR_SLEEPY_END_DEVICE | 
            Extended star mode device: An end device whose radio is turned off when not communicating to save power. The application must call emberPollForData() to receive messages. A node can be started as a sleepy end device using the emberJoinNetwork() or emberJoinNetworkExtended() API.  | 
         
| EMBER_DIRECT_DEVICE | 
            Direct mode device: A device able to send and receive messages from other devices in range on the same PAN ID, with no star topology restrictions. Such device does not relay messages. A node can be started as a direct device by using the emberJoinCommissioned() API.  | 
         
| EMBER_MAC_MODE_DEVICE | 
            MAC mode device: A device able to send and receive MAC-level messages. A node can be started as a MAC mode device by using the emberJoinCommissioned() , the emberJoinNetworkExtended() or the emberMacFormNetwork() API.  | 
         
| EMBER_MAC_MODE_SLEEPY_DEVICE | 
            MAC mode device: A sleepy device able to send and receive MAC-level messages. The radio on the device is turned off when not communicating. The application must call emberPollForData() to receive messages. A node can be started as a sleepy MAC mode device by using the emberJoinCommissioned() API or the emberJoinNetworkExtended() API.  | 
         
        Definition at line
        
         102
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberPhyType
| enum EmberPhyType | 
Define the PHY configuration of connect stack.
        Definition at line
        
         761
        
        of file
        
         ember-types.h
        
        .
       
◆ EmberTxStreamParameters
Function Documentation
◆ emberKeyContents()
| uint8_t* emberKeyContents | ( | EmberKeyData * | 
           
            key
           
           | 
          ) | 
This macro allows the programmer to gain access to the key data bytes of the EmberKeyData structure.
- Parameters
 - 
         
[in] keyA Pointer to an EmberKeyData structure.  
- Returns
 - uint8_t* Returns a pointer to the first byte of the key data.