EventActions Struct Reference
The static part of an event. Each event can be used with only one event queue. More...
      
       #include <
       
     
        ember-types.h
       
       >
      
         Data Fields | 
       |
| struct EventQueue_s * | queue | 
| void(* | handler )(struct Event_s *) | 
| void(* | marker )(struct Event_s *) | 
| const char * | name | 
The static part of an event. Each event can be used with only one event queue.
       Definition at line
       
        549
       
       of file
       
        ember-types.h
       
       .
      
Field Documentation
◆ handler
| void(* EventActions::handler) (struct Event_s *) | 
        Definition at line
        
         551
        
        of file
        
         ember-types.h
        
        .
       
◆ marker
| void(* EventActions::marker) (struct Event_s *) | 
        Definition at line
        
         552
        
        of file
        
         ember-types.h
        
        .
       
◆ name
| const char* EventActions::name | 
        Definition at line
        
         553
        
        of file
        
         ember-types.h
        
        .
       
◆ queue
| struct EventQueue_s * EventActions::queue | 
        Definition at line
        
         550
        
        of file
        
         ember-types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
ember-types.h