EmberEventData_S Struct Reference
Complete events with a control and a handler procedure. More...
      
       #include <
       
     
        ember-types.h
       
       >
      
         Data Fields | 
       |
| EmberEventControl * | control | 
| void(* | handler )(void) | 
Complete events with a control and a handler procedure.
An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.
       Definition at line
       
        597
       
       of file
       
        ember-types.h
       
       .
      
Field Documentation
◆ control
| EmberEventControl * EmberEventData_S::control | 
The control structure for the event.
        Definition at line
        
         599
        
        of file
        
         ember-types.h
        
        .
       
◆ handler
| void(* EmberEventData_S::handler) (void) | 
The procedure to call when the event fires.
        Definition at line
        
         601
        
        of file
        
         ember-types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
ember-types.h