EmberMacFrame Struct Reference
A structure that describes the addressing fields of a 802.15.4 frame. More...
      
       #include <
       
     
        ember-types.h
       
       >
      
         Data Fields | 
       |
| EmberMacAddress | srcAddress | 
| EmberMacAddress | dstAddress | 
| EmberPanId | srcPanId | 
| EmberPanId | dstPanId | 
| bool | srcPanIdSpecified | 
| bool | dstPanIdSpecified | 
A structure that describes the addressing fields of a 802.15.4 frame.
       Definition at line
       
        372
       
       of file
       
        ember-types.h
       
       .
      
Field Documentation
◆ dstAddress
| EmberMacAddress EmberMacFrame::dstAddress | 
An EmberMacAddress structure indicating the destination address of a MAC frame.
        Definition at line
        
         381
        
        of file
        
         ember-types.h
        
        .
       
◆ dstPanId
| EmberPanId EmberMacFrame::dstPanId | 
An EmberPanId struct indicating the destination PAN ID of a MAC frame. This field is meaningful only if dstPanIdSpecified is set to true.
        Definition at line
        
         391
        
        of file
        
         ember-types.h
        
        .
       
◆ dstPanIdSpecified
| bool EmberMacFrame::dstPanIdSpecified | 
True if the dstPanId field is set, false otherwise.
        Definition at line
        
         399
        
        of file
        
         ember-types.h
        
        .
       
◆ srcAddress
| EmberMacAddress EmberMacFrame::srcAddress | 
An EmberMacAddress structure indicating the source address of a MAC frame.
        Definition at line
        
         376
        
        of file
        
         ember-types.h
        
        .
       
◆ srcPanId
| EmberPanId EmberMacFrame::srcPanId | 
An EmberPanId struct indicating the source PAN ID of a MAC frame. This field is meaningful only if srcPanIdSpecified is set to true.
        Definition at line
        
         386
        
        of file
        
         ember-types.h
        
        .
       
◆ srcPanIdSpecified
| bool EmberMacFrame::srcPanIdSpecified | 
True if the srcPanId field is set, false otherwise.
        Definition at line
        
         395
        
        of file
        
         ember-types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
ember-types.h