Connect Stack Version
Macros to determine the stack version. More...
Macros |
|
| #define | EMBER_MAJOR_VERSION 3 |
|
The major version of the release. First digit of A.B.C.D.
More...
|
|
| #define | EMBER_MINOR_VERSION 2 |
|
The minor version of the release. Second digit of A.B.C.D.
More...
|
|
| #define | EMBER_PATCH_VERSION 3 |
|
The patch version of the release. Third digit of A.B.C.D.
More...
|
|
| #define | EMBER_SPECIAL_VERSION 0 |
|
Special version of the release. Fourth digit of A.B.C.D.
More...
|
|
| #define | EMBER_BUILD_NUMBER 239 |
|
Build number of the release. Should be stored on 2 bytes.
More...
|
|
| #define | EMBER_FULL_VERSION |
|
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
More...
|
|
| #define | EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA |
|
Version type of the release. EMBER_VERSION_TYPE_GA means generally available.
More...
|
|
| #define | SOFTWARE_VERSION EMBER_FULL_VERSION |
Detailed Description
Macros to determine the stack version.
Note that the Connect Stack version might not match the version of Flex SDK.
See
config.h
for source code.
Macro Definition Documentation
◆ EMBER_BUILD_NUMBER
| #define EMBER_BUILD_NUMBER 239 |
Build number of the release. Should be stored on 2 bytes.
Definition at line
66
of file
config.h
.
◆ EMBER_FULL_VERSION
| #define EMBER_FULL_VERSION |
config.h:61
config.h:48
config.h:56
config.h:43
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
Definition at line
72
of file
config.h
.
◆ EMBER_MAJOR_VERSION
| #define EMBER_MAJOR_VERSION 3 |
The major version of the release. First digit of A.B.C.D.
Definition at line
43
of file
config.h
.
◆ EMBER_MINOR_VERSION
| #define EMBER_MINOR_VERSION 2 |
The minor version of the release. Second digit of A.B.C.D.
Definition at line
48
of file
config.h
.
◆ EMBER_PATCH_VERSION
| #define EMBER_PATCH_VERSION 3 |
The patch version of the release. Third digit of A.B.C.D.
Patch versions are fully backwards compatible as long as the major and minor version matches.
Definition at line
56
of file
config.h
.
◆ EMBER_SPECIAL_VERSION
| #define EMBER_SPECIAL_VERSION 0 |
Special version of the release. Fourth digit of A.B.C.D.
Definition at line
61
of file
config.h
.
◆ EMBER_VERSION_TYPE
| #define EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA |
Version type of the release. EMBER_VERSION_TYPE_GA means generally available.
Definition at line
81
of file
config.h
.
◆ SOFTWARE_VERSION
| #define SOFTWARE_VERSION EMBER_FULL_VERSION |
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
Definition at line
86
of file
config.h
.