EmberEventControl Struct Reference
Control structure for events. More...
      
       #include <
       
     
        ember-types.h
       
       >
      
         Data Fields | 
       |
| EmberEventUnits | status | 
| EmberTaskId | taskid | 
| uint32_t | timeToExecute | 
Control structure for events.
This structure should not be accessed directly. It holds the event status (one of the EMBER_EVENT_ values) and the time left before the event fires.
       Definition at line
       
        579
       
       of file
       
        ember-types.h
       
       .
      
Field Documentation
◆ status
| EmberEventUnits EmberEventControl::status | 
The event's status, either inactive or the units for timeToExecute.
        Definition at line
        
         581
        
        of file
        
         ember-types.h
        
        .
       
◆ taskid
| EmberTaskId EmberEventControl::taskid | 
The task ID this event belongs to.
        Definition at line
        
         583
        
        of file
        
         ember-types.h
        
        .
       
◆ timeToExecute
| uint32_t EmberEventControl::timeToExecute | 
How long before the event fires. Units are always in milliseconds.
        Definition at line
        
         587
        
        of file
        
         ember-types.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       
ember-types.h