You are viewing documentation for version: 3.3 | 3.4 | Version History
◆ emberChildJoinHandler()
This handler is invoked at coordinator, range extender, or mac mode nodes when a new child has joined the device.
- Parameters
-
◆ emberFormNetwork()
Form a new network by becoming the coordinator. This API requires the parent-support library to be present.
- Parameters
-
[in] | parameters | An EmberNetworkParameters value that specifies the network parameters of the network to be formed. |
- Returns
- An
EmberStatus
value that indicates either the successful formation of the new network or an EmberStatus
value indicating the reason of failure.
◆ emberGetChildFlags()
Return an EmberChildFlags bitmask indicating the child flags of the child corresponding to the passed MAC address.
- Note
- Deprecated, use emberGetChildInfo instead
- Parameters
-
[in] | address | A pointer to an EmberMacAddress that specifies the MAC address of the child. |
[out] | flags | A pointer to an EmberChildFlags containing the child flags of the child corresponding to the passed MAC address. |
- Returns
- An
EmberStatus
value of EMBER_SUCCESS if the child was found in the child table, or another EmberStatus
value indicating the reason of failure.
◆ emberGetChildInfo()
Return info on the child corresponding to the passed MAC address.
- Note
- For star coordinators, if the input address is short, the corresponding child will also be searched in the list of devices connected through range extender. Long address and additional flags for these devices are not available to the coordinator.
- Parameters
-
[in] | address | A pointer to an EmberMacAddress that specifies the MAC address of the child (short or long). |
[out] | addressResp | A pointer to an EmberMacAddress that returns the other address (respectively long or short). |
[out] | flags | A pointer to an EmberChildFlags containing the child flags of the child corresponding to the passed MAC address. |
- Note
- Both out parameters are optional. If set to NULL, the API will at least indicate if the child was found in the network.
- Returns
- An
EmberStatus
value of EMBER_SUCCESS if the child was found in the child table, EMBER_CHILD_NOT_FOUND if it was not, or another EmberStatus
value indicating the reason of failure.
◆ emberPurgeIndirectMessages()
Purge all indirect transmissions from the indirect message queue.
- Returns
- an
EmberStatus
value of EMBER_SUCCESS if all indirect messages were purged, or another EmberStatus
value indicating the reason of failure.
◆ emberRemoveChild()
Remove the node corresponding to the passed MAC address from the child table.
- Parameters
-
[in] | address | A pointer to an EmberMacAddress that specifies the MAC address of the child to be removed. |
- Returns
- An
EmberStatus
value of EMBER_SUCCESS if the node was successfully removed from the child table, or another EmberStatus
value indicating the reason of failure.
◆ emberSetIndirectQueueTimeout()
EmberStatus emberSetIndirectQueueTimeout |
( |
uint32_t |
timeoutMs | ) |
|