Data Streams
Functions for reading, writing, etc data streams. More...
Functions |
|
| gos_result_t | gos_write ( gos_handle_t handle, const void *data, uint32_t size, bool auto_flush) |
|
Write data to stream.
More...
|
|
| gos_result_t | gos_read ( gos_handle_t handle, void *data, uint32_t max_size, uint32_t *bytes_read_ptr) |
|
Read data from stream.
More...
|
|
| gos_result_t | gos_read_with_buffer ( gos_handle_t handle, gos_buffer_t *buf) |
|
Read data from stream info
gos_buffer_t
.
More...
|
|
| gos_result_t | gos_close ( gos_handle_t handle) |
|
Close stream.
More...
|
|
| gos_result_t | gos_poll ( gos_handle_t handle, uint32_t *rx_available_ptr, uint32_t *tx_available_ptr) |
|
Poll stream for RX and TX buffer available.
More...
|
|
Detailed Description
Functions for reading, writing, etc data streams.
Function Documentation
◆ gos_close()
| gos_result_t gos_close | ( | gos_handle_t |
handle
|
) |
Close stream.
See Gecko OS Command API documentation: stream_close .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to close (use -1 to close all streams)
- Returns
- gos_result_t result of api call
◆ gos_poll()
| gos_result_t gos_poll | ( | gos_handle_t |
handle,
|
| uint32_t * |
rx_available_ptr,
|
||
| uint32_t * |
tx_available_ptr
|
||
| ) |
Poll stream for RX and TX buffer available.
This polls the given stream and returns if it has data to be read and available TX buffer space.
- Note
-
Set the
rx_available_ptrand/ortx_available_ptrarg NULL to ignore the parameter. - Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to poll [out] rx_available_ptrPointer to hold number of bytes available to read [out] tx_available_ptrPointer to hold available TX buffer space
- Returns
- gos_result_t result of api call
◆ gos_read()
| gos_result_t gos_read | ( | gos_handle_t |
handle,
|
| void * |
data,
|
||
| uint32_t |
max_size,
|
||
| uint32_t * |
bytes_read_ptr
|
||
| ) |
Read data from stream.
See Gecko OS Command API documentation: stream_read .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [out] dataBuffer to hold read data [in] max_sizeMaximum amount of data to read [out] bytes_read_ptrPointer to hold actual amount of data read (set NULL if not used)
- Returns
- gos_result_t result of api call
◆ gos_read_with_buffer()
| gos_result_t gos_read_with_buffer | ( | gos_handle_t |
handle,
|
| gos_buffer_t * |
buf
|
||
| ) |
Read data from stream info gos_buffer_t .
This has similar functionality as gos_read() except a gos_buffer_t is passed as an argument allowing for zero memory copies.
Only the 'size' field of the given gos_buffer_t argument should be populated with the maximum amount of data to read. The 'data' field should be NULL. When the API call returns:
- the 'size' field is updated with the amount of data actually read
- the 'data' field will be populated with the data pointer (if data was available)
Example usage:
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [out] bufBuffer to hold read data
- Returns
- gos_result_t result of api call
◆ gos_write()
| gos_result_t gos_write | ( | gos_handle_t |
handle,
|
| const void * |
data,
|
||
| uint32_t |
size,
|
||
| bool |
auto_flush
|
||
| ) |
Write data to stream.
See Gecko OS Command API documentation: stream_write .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [in] dataData to write to stream [in] sizeSize of data in bytes to write [in] auto_flushIf true, only flush data when the internal buffer is full, false flush the data immediately
- Returns
- gos_result_t result of api call