Macros
Log file specific macros. More...
Macros | |
#define | GOS_LOG_FILE_RECORD_VALID_FLAG 0x8000 |
Flag in a log record indicating if the log record data is valid. | |
#define | GOS_LOG_FILE_IS_VALID(header) (~((gos_log_file_header_t)header) & GOS_LOG_FILE_RECORD_VALID_FLAG) |
Helper to test if a log record is valid. | |
#define | GOS_LOG_FILE_GET_LENGTH(header) (((gos_log_file_header_t)header) & ~GOS_LOG_FILE_RECORD_VALID_FLAG) |
Helper to return the length of a log record. | |
#define | GOS_LOG_FILE_GET_NEXT -1 |
Used with gos_file_read_log() to read the next available log record. | |
Detailed Description
Log file specific macros.