Timer
RTOS timer functions. More...
Functions |
|
| gos_result_t | gos_rtos_timer_init (gos_timer_t *timer, uint32_t period_ms, gos_timer_handler_t callback, void *arg) |
|
Initializes a RTOS timer.
More...
|
|
| gos_result_t | gos_rtos_timer_deinit (gos_timer_t *timer) |
|
De-initialise a RTOS timer.
More...
|
|
| gos_result_t | gos_rtos_timer_start (gos_timer_t *timer) |
|
Starts a RTOS timer running.
More...
|
|
| gos_result_t | gos_rtos_timer_stop (gos_timer_t *timer) |
|
Stops a running RTOS timer.
More...
|
|
| gos_result_t | gos_rtos_timer_update (gos_timer_t *timer, uint32_t period_ms) |
|
Update timer's period.
More...
|
|
| gos_result_t | gos_rtos_timer_is_running (gos_timer_t *timer) |
|
Check if an RTOS timer is running.
More...
|
|
Detailed Description
RTOS timer functions.
Function Documentation
◆ gos_rtos_timer_deinit()
| gos_result_t gos_rtos_timer_deinit | ( | gos_timer_t * |
timer
|
) |
De-initialise a RTOS timer.
Deletes a RTOS timer created with gos_rtos_timer_init()
- Note
- This will automatically stop the timer if it's actively running.
- Parameters
-
[in] timer: Pointer to the RTOS timer handle
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_timer_init()
| gos_result_t gos_rtos_timer_init | ( | gos_timer_t * |
timer,
|
| uint32_t |
period_ms,
|
||
| gos_timer_handler_t |
callback,
|
||
| void * |
arg
|
||
| ) |
Initializes a RTOS timer.
Initialises a periodic RTOS timer.
- Note
- Timer does not start running until gos_rtos_timer_start() is called.
-
The timer callback runs in a high priority context. For this reason, it is extremely important to NOT specify too small of a
period_ms. A smallperiod_msplaces a large overhead on the system which may cause it to become unstable. Periods greater than 100 milliseconds are recommended.
- Parameters
-
[in] timer: Pointer to the timer handle to be initialised [in] period_ms: Timer period in milliseconds [in] callback: Callback function that is called each time the timer expires [in] arg: Argument that will be passed to the callback function
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_timer_is_running()
| gos_result_t gos_rtos_timer_is_running | ( | gos_timer_t * |
timer
|
) |
Check if an RTOS timer is running.
This returns GOS_SUCCESS if the timer is running. It return GOS_ERROR if the timer is NOT running.
- Parameters
-
[in] timer: Pointer to the RTOS timer handle
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_timer_start()
| gos_result_t gos_rtos_timer_start | ( | gos_timer_t * |
timer
|
) |
Starts a RTOS timer running.
Starts a RTOS timer running. Timer must have been previously initialised with gos_rtos_timer_init()
- Note
- If the timer is already running, this will effectively restart the timer.
- Parameters
-
[in] timer: Pointer to the timer handle to start
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_timer_stop()
| gos_result_t gos_rtos_timer_stop | ( | gos_timer_t * |
timer
|
) |
Stops a running RTOS timer.
Stops a running RTOS timer. Timer must have been previously started with gos_rtos_timer_start()
- Parameters
-
[in] timer: Pointer to the timer handle to stop
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_timer_update()
| gos_result_t gos_rtos_timer_update | ( | gos_timer_t * |
timer,
|
| uint32_t |
period_ms
|
||
| ) |
Update timer's period.
This updates a timer's period.
- Note
- If the timer is actively running then this restarts the timer.
- Parameters
-
[in] timer: Pointer to the timer handle to update [in] period_ms: Timer's new period in milliseconds
- Returns
- Result of API call, gos_result_t