Powersave

Functions that reduce power consumption. More...

Data Structures

struct gos_powersave_sleep_options_t

Functions

gos_result_t gos_powersave_sleep (const gos_powersave_sleep_options_t *options)
Put module into deep sleep. More...

Detailed Description

Functions that reduce power consumption.

Function Documentation

◆ gos_powersave_sleep()

gos_result_t gos_powersave_sleep ( const gos_powersave_sleep_options_t * options )

Put module into deep sleep.

See Gecko OS Command API documentation: sleep .

Note
Leave the options argument NULL to use the configured Gecko OS settings
Parameters
[in] options Options for how the device should wakeup, see gos_powersave_sleep_options_t , leave NULL to use configured Gecko OS settings
Returns
gos_result_t result of API