Interface

Functions for starting/stop WLAN & SoftAP interfaces. More...

Modules

Types
Network Interface Types.
Macros
Network interface specific macros.

Functions

gos_result_t gos_network_set_credentials ( gos_interface_t interface, const char *ssid, const char *password, bool save_to_nvm)
Set the interface's network credentials. More...
gos_result_t gos_network_get_credentials ( gos_interface_t interface, gos_ssid_t *ssid, gos_buffer_t *password)
Get the interface's network credentials. More...
gos_result_t gos_network_get_security ( gos_interface_t interface, gos_security_t *security_ptr)
Get the current security of the interface. More...
gos_result_t gos_network_up ( gos_interface_t interface, bool block)
Bring network interface up. More...
gos_result_t gos_network_down ( gos_interface_t interface)
Bring network interface down. More...
gos_result_t gos_network_restart ( gos_interface_t interface)
Restart network interface. More...
bool gos_network_is_up ( gos_interface_t interface)
Return status of network interface. More...
bool gos_network_is_permanent_down (void)
Return if the network interface is permanently down, this occurs when the module is being rebooted. More...
gos_interface_t gos_network_get_default_interface (void)
Return the currently active default network interface. More...
gos_result_t gos_network_set_default_interface ( gos_interface_t interface)
Set the default network interface. More...
gos_wlan_result_t gos_network_get_wlan_join_result (void)
Return the result of the most recent WLAN join attempt. More...
const char * gos_network_get_wlan_join_result_str (void)
Return the result string of the most recent WLAN join attempt. More...
gos_network_status_t gos_network_get_status ( gos_interface_t interface)
Return the current interface status. More...
gos_result_t gos_network_close_all_streams ( gos_interface_t interface)
Close all data streams on specified network interface. More...
gos_result_t gos_network_softap_client_list ( gos_softap_client_t *client_list, uint32_t *client_count)
Return list of SoftAP clients. More...
gos_result_t gos_network_softap_deauth_client ( gos_mac_t *mac, gos_deauth_reason_t reason)
Deauthenticate SoftAP client. More...
gos_result_t gos_network_register_event_handler ( gos_interface_t interface, gos_network_handler_t handler)
Register network event handler. More...
gos_result_t gos_network_register_softap_event_handler ( gos_softap_event_handler_t handler)
Register SoftAP client event handler. More...
void gos_network_set_softap_domain_list (const char *domain_list)
Set list of domain names DNS server will resolve. More...

Detailed Description

Functions for starting/stop WLAN & SoftAP interfaces.

Function Documentation

◆ gos_network_close_all_streams()

gos_result_t gos_network_close_all_streams ( gos_interface_t interface )

Close all data streams on specified network interface.

Parameters
[in] interface gos_interface_t the interface to close all streams on
Returns
gos_result_t result of api call

◆ gos_network_down()

gos_result_t gos_network_down ( gos_interface_t interface )

Bring network interface down.

See Gecko OS Command API documentation: network_down .

Parameters
[in] interface gos_interface_t the interface to bring down
Returns
gos_result_t result of api call

◆ gos_network_get_credentials()

gos_result_t gos_network_get_credentials ( gos_interface_t interface,
gos_ssid_t * ssid,
gos_buffer_t * password
)

Get the interface's network credentials.

This returns the current credentials for the given network interface.

Note
The supplied password buffer should be at least 64 bytes.
Parameters
[in] interface Interface to retrieve network credentials. See gos_interface_t
[out] ssid gos_ssid_t To be populated with interface's current SSID.
[out] password To be populated with interface's current password, the supplied buffer should be at least 64 chars
Returns
gos_result_t result of api call

◆ gos_network_get_default_interface()

gos_interface_t gos_network_get_default_interface ( void )

Return the currently active default network interface.

Returns
gos_interface_t the currently configured default network interface
Examples:
network/http_server/main.c , utility/msgpack/read_write_buffer.c , and utility/msgpack/read_write_stream.c .

◆ gos_network_get_security()

gos_result_t gos_network_get_security ( gos_interface_t interface,
gos_security_t * security_ptr
)

Get the current security of the interface.

Parameters
interface Interface to retrieve network security
security_ptr Pointer to gos_security_t to be populated with network's security
Returns
gos_result_t result of api call

◆ gos_network_get_status()

gos_network_status_t gos_network_get_status ( gos_interface_t interface )

Return the current interface status.

See gos_network_status_t for more info.

Parameters
interface Network interface, see gos_interface_t
Returns
Current interface status, see gos_network_status_t

◆ gos_network_get_wlan_join_result()

gos_wlan_result_t gos_network_get_wlan_join_result ( void )

Return the result of the most recent WLAN join attempt.

See gos_wlan_result_t for more info.

Returns
Result of last join attempt, see gos_wlan_result_t

◆ gos_network_get_wlan_join_result_str()

const char* gos_network_get_wlan_join_result_str ( void )

Return the result string of the most recent WLAN join attempt.

See gos_wlan_result_t for more info.

Returns
Result of last join attempt as string, see gos_wlan_result_t

◆ gos_network_is_permanent_down()

bool gos_network_is_permanent_down ( void )

Return if the network interface is permanently down, this occurs when the module is being rebooted.

Returns
true if the network interface is permanently down, false else

◆ gos_network_is_up()

bool gos_network_is_up ( gos_interface_t interface )

Return status of network interface.

Parameters
[in] interface gos_interface_t the interface to check status of
Returns
true is network interface is up, false else
Examples:
cloud/coap_demo/main.c , network/tcp_client/main.c , network/uart_tcp_client/main.c , network/udp_client/main.c , network/websocket_client/main.c , and wifi/device_setup/main.c .

◆ gos_network_register_event_handler()

gos_result_t gos_network_register_event_handler ( gos_interface_t interface,
gos_network_handler_t handler
)

Register network event handler.

Note
The event handler executes in the app thread context
Parameters
[in] interface gos_interface_t the interface to register handler with
[in] handler gos_network_handler_t to be called on network interface event
Returns
gos_result_t result of api call
Examples:
wifi/device_setup/main.c .

◆ gos_network_register_softap_event_handler()

gos_result_t gos_network_register_softap_event_handler ( gos_softap_event_handler_t handler )

Register SoftAP client event handler.

Note
The event handler executes in the app thread context
Parameters
[in] handler gos_softap_event_handler_t to be called on softap client event
Returns
gos_result_t result of api call
Examples:
network/softap_tcp_server/main.c .

◆ gos_network_restart()

gos_result_t gos_network_restart ( gos_interface_t interface )

Restart network interface.

See Gecko OS Command API documentation: network_restart .

Parameters
[in] interface gos_interface_t the interface to restart
Returns
gos_result_t result of api call
Examples:
cloud/coap_demo/main.c .

◆ gos_network_set_credentials()

gos_result_t gos_network_set_credentials ( gos_interface_t interface,
const char * ssid,
const char * password,
bool save_to_nvm
)

Set the interface's network credentials.

This sets the network credentials for the given interface.

Note
If save_to_nvm is false, the credentials are cached in RAM only. If save_to_nvm is true, the credentials are ALSO saved to NVM. Any other currently cached settings are also saved to NVM.
Parameters
[in] interface The network interface, see gos_interface_t
[in] ssid The network name, leave NULL to clear the interface's SSID
[in] password The network password, optional, leave NULL to clear the interface's password
[in] save_to_nvm Save credentials to NVM to they persist through reboots/powercycles
Returns
gos_result_t result of api call

◆ gos_network_set_default_interface()

gos_result_t gos_network_set_default_interface ( gos_interface_t interface )

Set the default network interface.

Note
The default interface will NOT update until the previous default interface is brought down.
Returns
gos_result_t result of api call

◆ gos_network_set_softap_domain_list()

void gos_network_set_softap_domain_list ( const char * domain_list )

Set list of domain names DNS server will resolve.

This set a list of domain names the SoftAP's DNS server will resolve. The specified list overrides the Gecko OS setting: softap.dns_server.url

Parameters
[in] domain_list Comma seperated list of domain names

◆ gos_network_softap_client_list()

gos_result_t gos_network_softap_client_list ( gos_softap_client_t * client_list,
uint32_t * client_count
)

Return list of SoftAP clients.

The supplied client_list argument should be a buffer large enough to hold all associated clients. e.g.

gos_softap_client_t client_list[GOS_MAX_SOFTAP_CLIENTS];
Parameters
[out] client_list Buffer containing list of associated client's information
[out] client_count Pointer to hold number of client's associated, leave NULL if unused
Returns
gos_result_t result of api call

◆ gos_network_softap_deauth_client()

gos_result_t gos_network_softap_deauth_client ( gos_mac_t * mac,
gos_deauth_reason_t reason
)

Deauthenticate SoftAP client.

This boots a softap client of the softap network.

Parameters
[in] mac MAC address of SoftAP client
[in] reason Reason for deauthenticating client, see gos_deauth_reason_t
Returns
gos_result_t result of api call

◆ gos_network_up()

gos_result_t gos_network_up ( gos_interface_t interface,
bool block
)

Bring network interface up.

See Gecko OS Command API documentation: network_up .

Parameters
[in] interface gos_interface_t the interface to bring up
[in] block true if API call should block until interface is brought up, false if it should return immediately
Returns
gos_result_t result of api call
Examples:
network/softap_tcp_server/main.c , network/tcp_client/main.c , network/uart_tcp_client/main.c , network/udp_client/main.c , network/websocket_client/main.c , and wifi/device_setup/main.c .