Contains information about a scan result. More...
Data Fields | |
gos_ssid_t | SSID |
Service Set Identification (i.e. Name of Access Point) | |
gos_mac_t | BSSID |
Basic Service Set Identification (i.e. MAC address of Access Point) | |
int16_t | signal_strength |
Receive Signal Strength Indication in dBm. <-90=Very poor, >-30=Excellent, 200=Off channel scan. | |
uint32_t | max_data_rate |
Maximum data rate in kilobits/s. | |
uint8_t | bss_type |
Network type, gos_bss_type_t. | |
uint32_t | security |
Security type, gos_security_t. | |
uint8_t | channel |
Radio channel that the AP beacon was received on. | |
uint8_t | band |
Radio band, gos_802_11_band_t. | |
uint8_t | on_channel |
True if scan result was recorded on the channel advertised in the packet. | |
struct gos_scan_result * | next |
Pointer to the next scan result. | |
Detailed Description
Contains information about a scan result.
- Examples:
- wifi/wifi_scan/main.c.