Hardware SPI data types. More...

Data Structures

struct gos_spi_message_t
SPI data message used by gos_spi_transfer() More...
struct gos_spi_device_t
SPI slave context used by gos_spi_transfer() More...

Enumerations

enum gos_spi_flag_t {
GOS_SPI_CLOCK_RISING_EDGE = ( 1 << 0 ),
GOS_SPI_CLOCK_FALLING_EDGE = ( 0 << 0 ),
GOS_SPI_CLOCK_IDLE_HIGH = ( 1 << 1 ),
GOS_SPI_CLOCK_IDLE_LOW = ( 0 << 1 ),
GOS_SPI_MSB_FIRST = ( 1 << 2 ),
GOS_SPI_LSB_FIRST = ( 0 << 2 ),
GOS_SPI_READ_AFTER_WRITE = ( 1 << 3 ),
GOS_SPI_NO_READ_AFTER_WRITE = ( 0 << 3 ),
GOS_SPI_KEEP_ASSERTED = ( 1 << 4 ),
GOS_SPI_DONT_KEEP_ASSERTED = ( 0 << 4 ),
GOS_SPI_HEXIFY = ( 1 << 5 ),
GOS_SPI_NO_HEXIFY = ( 0 << 5 ),
GOS_SPI_SLAVE_HW_NSS = ( 1 << 6 ),
GOS_SPI_SLAVE_NO_HW_NSS = ( 0 << 6 ),
GOS_SPI_QUAD_ENABLED = ( 1 << 6 ),
GOS_SPI_QUAD_DISABLED = ( 0 << 6 ),
GOS_SPI_MASTER_MODE = ( 0 << 7 ),
GOS_SPI_SLAVE_MODE = ( 1 << 7 ),
GOS_SPI_LOOPBACK_MODE = ( 1 << 8 ),
GOS_SPI_LCD_9BIT_MODE = ( 1 << 9 ),
GOS_SPI_ENABLE_AUTO_CS = ( 0 << 10 ),
GOS_SPI_DISABLE_AUTO_CS = ( 1 << 10 )
}
enum gos_spi_t {
GOS_SPI_0 ,
GOS_SPI_MAX
}

Detailed Description

Hardware SPI data types.

Enumeration Type Documentation

◆ gos_spi_flag_t

SPI device flags

Enumerator
GOS_SPI_CLOCK_RISING_EDGE

Data is valid on rising edge.

GOS_SPI_CLOCK_FALLING_EDGE

Data is valid on falling edge.

GOS_SPI_CLOCK_IDLE_HIGH

Clock idles high.

GOS_SPI_CLOCK_IDLE_LOW

Clock idles low.

GOS_SPI_MSB_FIRST

Shift Most-Significant Bit first.

GOS_SPI_LSB_FIRST

Shift Least-Significant Bit first.

GOS_SPI_READ_AFTER_WRITE

Allow for reading after writing flag When this is specified, when data is written to the SPI slave, the simultaneously read data is buffered. If this flag is not specified, when data is written, the read data is dropped.

Note
This is only used by the 'stream' APIs.
GOS_SPI_NO_READ_AFTER_WRITE

Don't read after writing. (i.e. drop read data while writing)

Note
This is only used by the 'stream' APIs.
GOS_SPI_KEEP_ASSERTED

Keep the slave-select signal asserted after the API call For the 'stream' API, this have has the following behavior: Sometimes it is necessary to keep the slave-select asserted between reads/writes. If this flag is not specified (i.e. GOS_SPI_DONT_KEEP_ASSERTED ) the slave-select is de-asserted after a read/write command. When this flag is specified, after a slave-select is asserted for a read/write command, it remains asserted until one of the events occurs:

  • close command is issued for the stream
  • A different slave-select gpio is specified as an argument to a read/write command
  • 0 bytes written to stream (i.e. write handle 0 )
GOS_SPI_DONT_KEEP_ASSERTED

De-select the slave-select signal after the API call.

GOS_SPI_HEXIFY

When set, input data to the write command is converted from a hex string to binary. Output data from the read command is converted from binary to a hex string.

Note
When this flag is set, up to rx buffer /2 -1 bytes may be read at a time
This flag is only used by the 'stream' API
GOS_SPI_NO_HEXIFY

Read/write data is always binary.

GOS_SPI_SLAVE_HW_NSS

GOS_SPI_SLAVE_HW_NSS.

GOS_SPI_SLAVE_NO_HW_NSS

GOS_SPI_SLAVE_NO_HW_NSS.

GOS_SPI_QUAD_ENABLED

GOS_SPI_QUAD_ENABLED.

GOS_SPI_QUAD_DISABLED

GOS_SPI_QUAD_DISABLED.

GOS_SPI_MASTER_MODE

GOS_SPI_MASTER_MODE.

GOS_SPI_SLAVE_MODE

GOS_SPI_SLAVE_MODE.

GOS_SPI_LOOPBACK_MODE

Local loopback mode enable.

GOS_SPI_LCD_9BIT_MODE

9 bit LCD mode. When set, this will set the number of bits per frame to 9, but will send and receive 8 bit data chunks for the application. The 9th bit (bit position 8) is controlled by the lcd_bit8 setting in gos_spi_device_t .

GOS_SPI_ENABLE_AUTO_CS

Enables automatic control of chip-select.

GOS_SPI_DISABLE_AUTO_CS

Disables automatic control of chip-select.

◆ gos_spi_t

Gecko OS SPI ID

Enumerator
GOS_SPI_0

This is just a placeholder, this is platform dependent.

GOS_SPI_MAX

Maximum number of SPIs the platform supports in Gecko OS.