WebSocket Client/Server
WebSocket client/server functions. More...
Modules |
|
| Types | |
|
WebSocket data types.
|
|
Functions |
|
| gos_result_t | gos_websocket_connect ( gos_interface_t interface, const char *host, gos_handle_t *handle_ptr) |
|
Connect to a remote websocket server.
More...
|
|
| gos_result_t | gos_websocket_connect_with_config (const gos_websocket_config_t *config, gos_handle_t *handle_ptr) |
|
Connect to a remote websocket server with configuration.
More...
|
|
| gos_result_t | gos_websocket_read ( gos_handle_t handle, void *data, uint32_t max_size, uint32_t *bytes_read_ptr) |
|
Read websocket stream data.
More...
|
|
| gos_result_t | gos_websocket_read_with_buffer ( gos_handle_t handle, gos_buffer_t *buffer) |
|
Read websocket stream data into buffer.
More...
|
|
| gos_result_t | gos_websocket_write ( gos_handle_t handle, const void *data, uint32_t size, bool continue_frame) |
|
Write websocket stream data.
More...
|
|
| gos_result_t | gos_websocket_disconnect ( gos_handle_t handle) |
|
Close websocket stream.
More...
|
|
| gos_result_t | gos_websocket_poll ( gos_handle_t handle, uint32_t *rx_bytes_available, uint32_t *tx_bytes_available) |
|
Poll websocket stream for RX data.
More...
|
|
| gos_result_t | gos_websocket_send_ping ( gos_handle_t handle, const void *data, uint32_t size) |
|
Send a 'Ping' to Websocket client or server.
More...
|
|
| gos_result_t | gos_websocket_client_read_frame ( gos_handle_t handle, gos_websocket_frame_t *frame, uint32_t timeout_ms) |
|
Read complete websocket frame.
More...
|
|
| void | gos_websocket_register_server_event_handlers ( gos_stream_event_handler_t connect, gos_stream_event_handler_t disconnect, gos_stream_event_handler_t receive) |
|
Register websocket server event handlers.
More...
|
|
| void | gos_websocket_register_client_event_handlers ( gos_handle_t handle, gos_stream_event_handler_t disconnect, gos_stream_event_handler_t receive) |
|
Register websocket client event handlers.
More...
|
|
| gos_result_t | gos_websocket_get_client_info ( gos_handle_t handle, char *host_buffer, uint32_t host_buffer_len, uint16_t *local_port_ptr, uint16_t *remote_port_ptr) |
|
Get Websocket client info.
More...
|
|
Detailed Description
WebSocket client/server functions.
Function Documentation
◆ gos_websocket_client_read_frame()
| gos_result_t gos_websocket_client_read_frame | ( | gos_handle_t |
handle,
|
| gos_websocket_frame_t * |
frame,
|
||
| uint32_t |
timeout_ms
|
||
| ) |
Read complete websocket frame.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
◆ gos_websocket_connect()
| gos_result_t gos_websocket_connect | ( | gos_interface_t |
interface,
|
| const char * |
host,
|
||
| gos_handle_t * |
handle_ptr
|
||
| ) |
Connect to a remote websocket server.
This opens a websocket client stream.
See Gecko OS Command API documentation: websocket_client .
- Parameters
-
interfaceThe network interface to open connect hostThe remote websocket server's URL handle_ptrThe stream handle of the opened websocket client stream
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c .
◆ gos_websocket_connect_with_config()
| gos_result_t gos_websocket_connect_with_config | ( | const gos_websocket_config_t * |
config,
|
| gos_handle_t * |
handle_ptr
|
||
| ) |
Connect to a remote websocket server with configuration.
See Gecko OS Command API documentation: websocket_client .
This does the same thing as gos_websocket_connect() but allows for additional configuration. See gos_websocket_config_t for optional configuration settings.
- Parameters
-
configWebsocket client configuration handle_ptrThe stream handle of the opened websocket client stream
- Returns
- gos_result_t result of api call
◆ gos_websocket_disconnect()
| gos_result_t gos_websocket_disconnect | ( | gos_handle_t |
handle
|
) |
Close websocket stream.
See Gecko OS Command API documentation: stream_close .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to close
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c .
◆ gos_websocket_get_client_info()
| gos_result_t gos_websocket_get_client_info | ( | gos_handle_t |
handle,
|
| char * |
host_buffer,
|
||
| uint32_t |
host_buffer_len,
|
||
| uint16_t * |
local_port_ptr,
|
||
| uint16_t * |
remote_port_ptr
|
||
| ) |
Get Websocket client info.
See Gecko OS Command API documentation: stream_list .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleClient stream handle [in] host_bufferBuffer to hold client host domain or IP address string [in] host_buffer_lenLength of host_buffer[in] local_port_ptrPointer to hold client's local port, leave NULL to ignore [in] remote_port_ptrPointer to hold client's remote port, leave NULL to ignore
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_server/main.c .
◆ gos_websocket_poll()
| gos_result_t gos_websocket_poll | ( | gos_handle_t |
handle,
|
| uint32_t * |
rx_bytes_available,
|
||
| uint32_t * |
tx_bytes_available
|
||
| ) |
Poll websocket stream for RX data.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to poll [out] rx_bytes_availablePointer to hold number of bytes available to read [out] tx_bytes_availablePointer to hold available TX buffer space
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c .
◆ gos_websocket_read()
| gos_result_t gos_websocket_read | ( | gos_handle_t |
handle,
|
| void * |
data,
|
||
| uint32_t |
max_size,
|
||
| uint32_t * |
bytes_read_ptr
|
||
| ) |
Read websocket stream data.
See Gecko OS Command API documentation: stream_read .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [out] dataBuffer to hold read data [in] max_sizeMaximum amount of data to read [out] bytes_read_ptrPointer to hold actual amount of data read (set NULL if not used)
- Returns
- gos_result_t result of api call
◆ gos_websocket_read_with_buffer()
| gos_result_t gos_websocket_read_with_buffer | ( | gos_handle_t |
handle,
|
| gos_buffer_t * |
buffer
|
||
| ) |
Read websocket stream data into buffer.
See gos_read_with_buffer() for more information.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handleStream handle bufferBuffer to specify how much data to read, then return how much data was read with pointer to data
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c , and network/websocket_server/main.c .
◆ gos_websocket_register_client_event_handlers()
| void gos_websocket_register_client_event_handlers | ( | gos_handle_t |
handle,
|
| gos_stream_event_handler_t |
disconnect,
|
||
| gos_stream_event_handler_t |
receive
|
||
| ) |
Register websocket client event handlers.
The corresponding event handlers will be called on the given websocket clients event. See gos_websocket_connect() to open a websocket client.
- Note
- The event handlers execute in the app thread context
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handleStream handle of websocket client stream (returned by gos_websocket_connect() ) disconnectWebsocket client disconnect event handler receiveWebsocket client data received event handler
- Examples:
- network/websocket_client/main.c .
◆ gos_websocket_register_server_event_handlers()
| void gos_websocket_register_server_event_handlers | ( | gos_stream_event_handler_t |
connect,
|
| gos_stream_event_handler_t |
disconnect,
|
||
| gos_stream_event_handler_t |
receive
|
||
| ) |
Register websocket server event handlers.
The following event handler will be called on the corresponding websocket server events. Set to NULL to disable the event handler.
- Note
- The event handlers execute in the app thread context
- Parameters
-
connectWebsocket client connect event handler disconnectWebsocket client disconnect event handler receiveWebsocket client data received event handler
- Examples:
- network/websocket_server/main.c .
◆ gos_websocket_send_ping()
| gos_result_t gos_websocket_send_ping | ( | gos_handle_t |
handle,
|
| const void * |
data,
|
||
| uint32_t |
size
|
||
| ) |
Send a 'Ping' to Websocket client or server.
This sends a 'Ping' with an optional data payload to the websocket client/server. If no data payload is required then leave the 'size' paramater zero.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handleHandle of websocket client/server stream dataOptional ping data payload, leave NULL if unused sizeSize of optional data payload, leave zero if unused
- Returns
- gos_result_t result of api call
◆ gos_websocket_write()
| gos_result_t gos_websocket_write | ( | gos_handle_t |
handle,
|
| const void * |
data,
|
||
| uint32_t |
size,
|
||
| bool |
continue_frame
|
||
| ) |
Write websocket stream data.
See Gecko OS Command API documentation: stream_write .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [in] dataData to write to stream [in] sizeSize of data in bytes to write [in] continue_frameIf true then sends 'continued' websocket frame, false send 'final' websocket frame
- Returns
- gos_result_t result of api call
- Examples:
- network/websocket_client/main.c , and network/websocket_server/main.c .