gos_http_response_t Struct Reference

HTTP response struct used by gos_http_receive_response() More...

Data Fields

int version
 
int code
 HTTP response code.
 
int content_length
 
char * headers [GOS_HTTP_BASIC_HEADER_COUNT]
 'Basic' HTTP response headers, see gos_http_basic_header_t
 
gos_http_response_header_theader_list
 
uint8_t * buffer
 Allocated HTTP response headers buffer (system use only)
 

Detailed Description

Field Documentation

◆ content_length

int gos_http_response_t::content_length

The response body length

Note
-1 means the response body is chunked
Examples:
network/http_methods/http_delete.c, network/http_methods/http_get.c, network/http_methods/http_post.c, and network/http_methods/http_put.c.

◆ header_list

gos_http_response_header_t* gos_http_response_t::header_list

Linked list of additional response headers

Note
Must set GOS_HTTP_RESPONSE_ALL_HEADERS flag to return additional headers

◆ version

int gos_http_response_t::version

The version of the HTTP response,

  • 0 = HTTP/1.0
  • 1 = HTTP/1.1