Gecko OS Studio Quickstart
Follow the steps below to prepare your device and set up your Gecko OS development environment for developing Gecko OS Apps.
Note : You can use the GSS to set up your device with the latest Gecko OS firmware .
Special terms used in Gecko OS documentation
- GSS - Gecko OS Studio.
- App - in the Gecko OS context, app refers to a Gecko OS Native 'C' API application.
Special Notes
- The current GSS version does not support file or directory names containing spaces.
Downloading GSS
Download GSS for your operating system:
Installing GSS
Run the downloaded executable to install GSS. The installer removes and replaces any previous version.
Getting Started with GSS
Open GSS.
Log in to your Silabs account. If you do not already have a free account, click
Create an Account
and follow the steps to create one.
After you log in, GSS displays the welcome screen.
Selecting Your Device
Click
Device
in the menu to open the Device tab:
Connect the device to the USB socket and power it up. GSS detects the device. If it is the only Silabs device detected, GSS selects it automatically:
When the device is selected, GSS moves to the
Projects
tab.
You may wish to set up Gecko OS on your device, with no associated Gecko OS App. If so, follow through the steps below in Setting Up Your Device with Gecko OS .
Otherwise, skip to Selecting Your Project .
Setting Up Your Device with Gecko OS
Select AEM Power Source
The WSTK power source selector switch should be set to the AEM (Advanced Energy Monitor) position. The AEM provides features required by the GSS.
Flash Gecko OS to Your Device
On GSS, click the
Setup Device with Gecko OS
button to flash the latest version of Gecko OS to your device.
GSS takes a few seconds to set up your device.
When the
Device Ready
notice appears, your device has a standard Gecko OS image for your platform.
You can now connect to the device via the UART and use the Command API. See Opening a Gecko OS Terminal .
When you move to other GSS screens, the
Setup Device with Gecko OS
button appears again. There is no need to set up the device again.
You can also move on in GSS to create a project, build it and download it to your device.
Selecting Your Project
GSS opens the Projects screen:
Hello World
We demonstrate building and downloading a project with the
Hello World
example project.
Choose
Clone Example
:
On the
Clone Example
screen,
- specify your preferred workspace path
-
scroll down through the examples, choose the
intro/hello_worldproject, and clickClone:
GSS creates the project, showing progress:
Finally the Project Created screen appears.
In the specified workspace directory, GSS created the
sdk-wgm160p-x.x.x-x
directory containing sdk files, and the
hello_world
project directory.
Choose
Open Project Folder
to open the project directory. You can view and edit the project source files in the IDE or text editor of your choice. For example, here is
main.c
:
When you are ready to build, in the
Project Created
screen, choose
Program Selected Device
to build the project and write the hello world code to the device.
The hello_world app runs each time the device reboots.
To view the output you can use a serial terminal program such as TeraTerm. See Opening a Gecko OS terminal .
In the case of the
hello_world
project, the App prints "Hello world!!" to the terminal.
[Ready]
>
Hello world!!
Browse the examples to see how Gecko OS Native C APIs are used in a range of applications. You can clone an example even when you have no physical development platform. Just choose the required target platform, clone the example and press
Open Project Folder
in the
Project Created
screen.
Using the IDE
On the Project Created screen, you can choose
Install IDE & Open Project
.
Alternatively, to install the Integrated Development Environment (IDE), choose the
Tools
tab and click
Install Gecko OS IDE
.
With the IDE installed, you can choose
Open in IDE
in the
Project Created
screen.
In the IDE you can edit, build, download, run and debug your App. You can also browse through the source for all example applications, under the
sdk-wgm160p-x.x.x-x
project, applications folder.
To build your app in the IDE, in the Project Explorer panel, right click on the project to build. In this case the project is
hello_world
. In the context menu, choose one of the build options:
-
Build Project- compile App from source -
Clean Project- remove intermediate output from previous builds -
Build / Download- compile App and download to device -
Build / Download / Run- compile App, download to device and run the App -
Build / Download / Debug- compile App, download to device and run the App with debugging options
The IDE builds the project and displays output in the build console.
If you have a Gecko OS terminal connected to the board port, the App output appears on the terminal, similar to the following:
[Ready]
SILABS-HELLO-0.0.0-local, Gecko_OS-STANDARD-4.0.17-1380, WGM160P
Hello world!!
LOCAL>
Downloading Resources
Choose the
Download Resources
option on the project
Gecko OS
menu to download resources to your Gecko OS device. Resources include the webapp, Wi-Fi firmware and other resources related to Gecko OS and your App.
Command Line Make
The GSS IDE uses the make utility to build Apps. Using make from the command line can provide additional options. See Using Gecko OS Make .