mDNS functions More...

Modules

Types
mDNS data types

Functions

mdns_service_details_t gos_mdns_setup_service_details ( gos_mdns_service_details_t *service_details, const char *service_name, const char *instance_name, uint16_t port, uint16_t priority, uint16_t weight, uint16_t ttl, const char *txt_buffer, uint16_t max_txt_size)
populates mdns_service_details_t structure with parameters. More...
mdns_service_handle_t gos_mdns_service_register ( gos_interface_t interface, gos_mdns_service_details_t *service_details)
Register an mDNS service. More...
gos_result_t gos_mdns_service_unregister ( mdns_service_handle_t service_handle)
Unregister an mDNS service. More...

Detailed Description

mDNS functions

Function Documentation

◆ gos_mdns_service_register()

mdns_service_handle_t gos_mdns_service_register ( gos_interface_t interface,
gos_mdns_service_details_t * service_details
)

Register an mDNS service.

This registers an mDNS service

Parameters
interface gos_interface_t
service_details gos_mdns_service_details_t
Returns
mdns_service_handle_t the service handle

◆ gos_mdns_service_unregister()

gos_result_t gos_mdns_service_unregister ( mdns_service_handle_t service_handle )

Unregister an mDNS service.

This unregisters an mDNS service previously registered with gos_mdns_service_register()

Parameters
service_handle service handle returned by gos_mdns_service_register() when service was registered
Returns
gos_result_t the result of unregistering the service

◆ gos_mdns_setup_service_details()

mdns_service_details_t gos_mdns_setup_service_details ( gos_mdns_service_details_t * service_details,
const char * service_name,
const char * instance_name,
uint16_t port,
uint16_t priority,
uint16_t weight,
uint16_t ttl,
const char * txt_buffer,
uint16_t max_txt_size
)

populates mdns_service_details_t structure with parameters.

This function formats the parameters required for mDNS and populates the service details, so that gos_mdns_service_register can be called

Parameters
service_details gos_mdns_service_details_t
service_name mDNS service name - must end with .local
instance_name name of the service instannce
port The TCP or UDP port on which the service is to be found.
priority The priority of the target host, lower value means more preferred
weight A relative weight for records with the same priority, higher value means more preferred
ttl Time to live, period of caching of the resource records
txt_buffer buffer for storing txt data
max_txt_size legnth of txt_buffer
Returns
gos_result_t the result of gos_mdns_setup_service_details()