Application NVM
Functions for reading/writing/loading NVM entries that are custom defined by Gecko OS applications. More...
Modules | |
Macros | |
Settings specific macros. | |
Enumerations | |
enum | gos_factory_reset_t { GOS_NVM_RESET_BACKUP, GOS_NVM_RESET_FACTORY, GOS_NVM_RESET_CACHE_ONLY } |
Functions | |
gos_result_t | gos_nvm_retrieve (gos_nvm_entry_header_t key, void **value_ptr) |
Retrieve a reference to an NVM cache entry. More... | |
gos_result_t | gos_nvm_update (gos_nvm_entry_header_t key, const void *new_value, bool force_set) |
Update the value of a NVM cache entry. More... | |
gos_result_t | gos_nvm_save (void) |
Save cached RAM NVM setting to NVM. More... | |
gos_result_t | gos_nvm_factory_reset (gos_factory_reset_t reset_type) |
Detailed Description
Functions for reading/writing/loading NVM entries that are custom defined by Gecko OS applications.
Enumeration Type Documentation
◆ gos_factory_reset_t
enum gos_factory_reset_t |
NVM Factory reset type
Function Documentation
◆ gos_nvm_factory_reset()
gos_result_t gos_nvm_factory_reset | ( | gos_factory_reset_t | reset_type | ) |
Factory reset the application's NVM settings
Refer to gos_factory_reset_t for the various reset types.
- Note
- This API does NOT return when GOS_NVM_RESET_FACTORY is used.
- This API will reset application NVM ONLY, Gecko OS Plugin and Kernel settings are NOT affected by the API. See gos_settings_factory_reset() to factory reset ALL settings
- Parameters
-
reset_type
The factory reset type, see gos_factory_reset_t
- Returns
- The result of the API, see gos_result_t
- Examples:
- system/application_nvm/main.c.
◆ gos_nvm_retrieve()
gos_result_t gos_nvm_retrieve | ( | gos_nvm_entry_header_t | key, |
void ** | value_ptr |
||
) |
Retrieve a reference to an NVM cache entry.
On Gecko OS startup, the NVM data is loaded into a cache. This API allows for retrieving a reference to the cached entry.
See GOS_NVM_GET() for a simplified version of this API.
- Parameters
-
key
NVM entry key, use GOS_NVM_KEY() to specify the key value_ptr
Pointer to hold NVM cache reference
- Returns
- Result of API, see gos_result_t
◆ gos_nvm_save()
gos_result_t gos_nvm_save | ( | void |
| ) |
Save cached RAM NVM setting to NVM.
This saves all data in the application's NVM RAM cache to NVM. All saved data will automatically be reload on powerup/startup.
- Note
- This API will save the Application's NVM ONLY, Gecko OS Plugin and Kernel settings are NOT affected by the API. See gos_settings_save() to save Plugin and Kernel settings.
- Returns
- Result of API, see gos_result_t
◆ gos_nvm_update()
gos_result_t gos_nvm_update | ( | gos_nvm_entry_header_t | key, |
const void * | new_value, |
||
bool | force_set |
||
) |
Update the value of a NVM cache entry.
This attempts to update the value of the specified NVM entry in cache. IfF the entry's key is not found and:
- force_set = false THEN this API fails
- force_set = true THEN this API creates a new entry in cache with the given value
See GOS_NVM_UPDATE() and GOS_NVM_UPDATE_FORCED() for simplified versions of this API.
- Note
- This API ONLY updates the NVM entry in cache. gos_nvm_save() must be used to save the cache to NVM.
- Parameters
-
key
NVM entry key, use GOS_NVM_KEY() to specify the key new_value
New value of NVM cache entry. The length of the value must NOT be longer than what was specified when the NVM entry key was defined using GOS_NVM_DEFINE_ENTRY() force_set
Set the new NVM value even if it doesn't exist, if this is false and the entry does not exist (i.e. no default value is defined) then this return @ GOS_NOT_FOUND
- Returns
- Result of API, see gos_result_t