APIs for accessing SPI master 'stream' functionality. More...

Functions

gos_result_t gos_spi_stream_configure ( gos_spi_t port, gos_gpio_t ss_gpio, gos_spi_flag_t flags, uint32_t clock_rate)
Configure SPI stream for communication with SPI slave. More...
gos_result_t gos_spi_stream_open ( gos_handle_t *handle_ptr, uint16_t rx_buffer_size)
Open SPI stream to slave device. More...
gos_result_t gos_spi_stream_write ( gos_handle_t handle, const void *data, uint32_t size)
Write data to slave device. More...
gos_result_t gos_spi_stream_read ( gos_handle_t handle, void *data, uint32_t max_size, uint32_t *bytes_read_ptr)
Read data from slave device. More...
gos_result_t gos_spi_stream_read_with_buffer ( gos_handle_t handle, gos_buffer_t *buffer)
Read SPI stream data into buffer. More...
gos_result_t gos_spi_stream_close ( gos_handle_t handle)
Close SPI stream. More...
gos_result_t gos_spi_stream_set_slave_select ( gos_handle_t handle, gos_gpio_t ss_gpio)
Switch SPI stream's slave device. More...

Detailed Description

APIs for accessing SPI master 'stream' functionality.

Function Documentation

◆ gos_spi_stream_close()

gos_result_t gos_spi_stream_close ( gos_handle_t handle )

Close SPI stream.

See Gecko OS Command API documentation: stream_close .

Note
Stream handles start at 1, max handle value is GOS_MAX_STREAMS
Parameters
[in] handle Handle of stream to close
Returns
gos_result_t result of api call

◆ gos_spi_stream_configure()

gos_result_t gos_spi_stream_configure ( gos_spi_t port,
gos_gpio_t ss_gpio,
gos_spi_flag_t flags,
uint32_t clock_rate
)

Configure SPI stream for communication with SPI slave.

See Gecko OS Command API documentation: spi_master_config .

Parameters
[in] port SPI peripheral port
[in] ss_gpio Slave-select gpio
[in] flags Configuration flags, see SPI_FLAG macros
[in] clock_rate SPI master clock
Returns
result of api call, see gos_result_t

◆ gos_spi_stream_open()

gos_result_t gos_spi_stream_open ( gos_handle_t * handle_ptr,
uint16_t rx_buffer_size
)

Open SPI stream to slave device.

See Gecko OS Command API documentation: spi_master_open .

Parameters
[out] handle_ptr Stream handle
[in] rx_buffer_size Size of RX buffer
Returns
result of api call, see gos_result_t

◆ gos_spi_stream_read()

gos_result_t gos_spi_stream_read ( gos_handle_t handle,
void * data,
uint32_t max_size,
uint32_t * bytes_read_ptr
)

Read data from slave device.

See Gecko OS Command API documentation: spi_master_open , stream_read .

Note
Stream handles start at 1, max handle value is GOS_MAX_STREAMS
Parameters
[in] handle Stream handle returned by API call
[out] data Buffer to hold read data
[in] max_size Maximum amount of data to read
[out] bytes_read_ptr Pointer to hold actual amount of data read (set NULL if not used)
Returns
gos_result_t result of api call

◆ gos_spi_stream_read_with_buffer()

gos_result_t gos_spi_stream_read_with_buffer ( gos_handle_t handle,
gos_buffer_t * buffer
)

Read SPI stream data into buffer.

See gos_read_with_buffer() for more information.

Note
Stream handles start at 1, max handle value is GOS_MAX_STREAMS
Parameters
handle Stream handle
buffer Buffer to specify how much data to read, then return how much data was read with pointer to data
Returns
gos_result_t result of api call

◆ gos_spi_stream_set_slave_select()

gos_result_t gos_spi_stream_set_slave_select ( gos_handle_t handle,
gos_gpio_t ss_gpio
)

Switch SPI stream's slave device.

A SPI stream can be associated with multiple SPI slaves. A SPI slave is configured with gos_spi_stream_configure() The configured SPI slave is then selected with this API

Note
Stream handles start at 1, max handle value is GOS_MAX_STREAMS
Parameters
[in] handle SPI stream handle
[in] ss_gpio GPIO of configured SPI slave
Returns
gos_result_t result of api call

◆ gos_spi_stream_write()

gos_result_t gos_spi_stream_write ( gos_handle_t handle,
const void * data,
uint32_t size
)

Write data to slave device.

See Gecko OS Command API documentation: spi_master_open , stream_write .

Note
Stream handles start at 1, max handle value is GOS_MAX_STREAMS
Parameters
[in] handle Stream handle returned by API call
[in] data Data to write to stream
[in] size Size of data in bytes to write
Returns
gos_result_t result of api call