MessagePack macros. More...

Macros

#define MSGPACK_BOOL(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t, boolean)
 
#define MSGPACK_INT8(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t, s)
 
#define MSGPACK_UINT8(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t, u)
 
#define MSGPACK_INT16(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t, s)
 
#define MSGPACK_UINT16(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t, u)
 
#define MSGPACK_INT32(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t, s)
 
#define MSGPACK_UINT32(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t, u)
 
#define MSGPACK_FLOAT(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t, flt)
 
#define MSGPACK_INT64(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t, s)
 
#define MSGPACK_UINT64(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t, u)
 
#define MSGPACK_DOUBLE(obj)   _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t, dbl)
 
#define MSGPACK_DICT(obj, key)   gos_msgpack_get_dict_object((gos_msgpack_object_dict_t*)obj, key, MSGPACK_TYPE_ANY)
 
#define MSGPACK_DICT_TYPE(obj, key, type)   gos_msgpack_get_dict_object((gos_msgpack_object_dict_t*)obj, key, MSGPACK_TYPE_ ## type)
 
#define MSGPACK_DICT_STR(obj, key)   (gos_msgpack_object_str_t*)MSGPACK_DICT_TYPE(obj, key, STR)
 
#define MSGPACK_DICT_BIN(obj, key)   (gos_msgpack_object_bin_t*)MSGPACK_DICT_TYPE(obj, key, BIN)
 
#define MSGPACK_DICT_DICT(obj, key)   (gos_msgpack_object_dict_t*)MSGPACK_DICT_TYPE(obj, key, DICT)
 
#define MSGPACK_DICT_ARRAY(obj, key)   (gos_msgpack_object_array_t*)MSGPACK_DICT_TYPE(obj, key, ARRAY)
 
#define MSGPACK_DICT_INT(obj, key)   MSGPACK_DICT_TYPE(obj, key, INT_OR_UINT)
 
#define MSGPACK_DICT_UINT(obj, key)   MSGPACK_DICT_TYPE(obj, key, INT_OR_UINT)
 
#define MSGPACK_ARRAY(obj, index)   gos_msgpack_get_array_object((gos_msgpack_object_array_t*)obj, index, MSGPACK_TYPE_ANY)
 
#define MSGPACK_ARRAY_TYPE(obj, index, type)   gos_msgpack_get_array_object((gos_msgpack_object_array_t*)obj, index, MSGPACK_TYPE_ ## type)
 
#define MSGPACK_ARRAY_DICT(obj, index)   (gos_msgpack_object_dict_t*)MSGPACK_ARRAY_TYPE(obj, index, DICT)
 
#define MSGPACK_ARRAY_ARRAY(obj, index)   (gos_msgpack_object_array_t*)MSGPACK_ARRAY_TYPE(obj, index, ARRAY)
 
#define MSGPACK_ARRAY_LENGTH(obj)   (((gos_msgpack_object_array_t*)obj)->count)
 
#define MSGPACK_ARRAY_STR(obj, index)   (gos_msgpack_object_str_t*)MSGPACK_ARRAY_TYPE(obj, index, STR)
 
#define MSGPACK_ARRAY_BIN(obj, index)   (gos_msgpack_object_bin_t*)MSGPACK_ARRAY_TYPE(obj, index, BIN)
 
#define MSGPACK_ARRAY_INT(obj, index)   MSGPACK_ARRAY_TYPE(obj, index, INT)
 
#define MSGPACK_ARRAY_UINT(obj, index)   MSGPACK_ARRAY_TYPE(obj, index, UINT)
 
#define MSGPACK_STR_VALUE(obj)   ((const gos_msgpack_object_str_t*)(obj))->data
 
#define MSGPACK_STR_LENGTH(obj)   ((const gos_msgpack_object_str_t*)(obj))->length
 
#define MSGPACK_STR_CMP(obj, str)   gos_msgpack_str_cmp((gos_msgpack_object_t*)obj, str)
 
#define MSGPACK_BIN_VALUE(obj)   ((const gos_msgpack_object_bin_t*)(obj))->data
 
#define MSGPACK_BIN_LENGTH(obj)   ((const gos_msgpack_object_bin_t*)(obj))->length
 
#define MSGPACK_BIN_CMP(obj, mem)   memcmp(MSGPACK_BIN_VALUE(obj), mem, MSGPACK_BIN_LENGTH(obj))
 
#define MSGPACK_INT(obj)   gos_msgpack_get_int(obj)
 
#define MSGPACK_UINT(obj)   gos_msgpack_get_uint(obj)
 
#define MSGPACK_LONG(obj, buffer)   gos_msgpack_get_long(obj, buffer)
 
#define MSGPACK_ULONG(obj, buffer)   gos_msgpack_get_ulong(obj, buffer)
 
#define MSGPACK_STR(obj, buffer, max_length)   gos_msgpack_get_str((gos_msgpack_object_t*)obj, buffer, max_length)
 
#define MSGPACK_BIN(obj, mem, max_length)   memcpy(mem, MSGPACK_BIN_VALUE(obj), MIN(max_length, MSGPACK_BIN_LENGTH(obj)))
 
#define MSGPACK_TO_STR(obj, buffer, max_length)   gos_msgpack_to_str((gos_msgpack_object_t*)obj, buffer, max_length)
 
#define MSGPACK_IS_NIL(obj)   _MSGPACK_IS_(obj, NIL)
 
#define MSGPACK_IS_BOOL(obj)   _MSGPACK_IS_(obj, BOOL)
 
#define MSGPACK_IS_INT8(obj)   _MSGPACK_IS_(obj, INT8)
 
#define MSGPACK_IS_UINT8(obj)   _MSGPACK_IS_(obj, UINT8)
 
#define MSGPACK_IS_INT16(obj)   _MSGPACK_IS_(obj, INT16)
 
#define MSGPACK_IS_UINT16(obj)   _MSGPACK_IS_(obj, UINT16)
 
#define MSGPACK_IS_INT32(obj)   _MSGPACK_IS_(obj, INT32)
 
#define MSGPACK_IS_UINT32(obj)   _MSGPACK_IS_(obj, UINT32)
 
#define MSGPACK_IS_INT64(obj)   _MSGPACK_IS_(obj, INT64)
 
#define MSGPACK_IS_UINT64(obj)   _MSGPACK_IS_(obj, UINT64)
 
#define MSGPACK_IS_UINT(obj)   gos_msgpack_object_is_type((gos_msgpack_object_t*)obj, MSGPACK_TYPE_UINT)
 
#define MSGPACK_IS_INT(obj)   gos_msgpack_object_is_type((gos_msgpack_object_t*)obj, MSGPACK_TYPE_INT)
 
#define MSGPACK_IS_FLOAT(obj)   _MSGPACK_IS_(obj, FLOAT)
 
#define MSGPACK_IS_DOUBLE(obj)   _MSGPACK_IS_(obj, DOUBLE)
 
#define MSGPACK_IS_STR(obj)   _MSGPACK_IS_(obj, STR)
 
#define MSGPACK_IS_BIN(obj)   _MSGPACK_IS_(obj, BIN)
 
#define MSGPACK_IS_DICT(obj)   _MSGPACK_IS_(obj, DICT)
 
#define MSGPACK_IS_ARRAY(obj)   _MSGPACK_IS_(obj, ARRAY)
 
#define MSGPACK_NIL   0xC0
 
#define MSGPACK_FALSE   0xC2
 
#define MSGPACK_TRUE   0xC3
 
#define MSGPACK_INIT_WITH_BUFFER(name, _buf, _len)
 
#define MSGPACK_INIT_CONTEXT_WITH_BUFFER(context, _buf, _len)
 
#define MSGPACK_INIT_WITH_WRITER(name, _writer, _user)
 
#define MSGPACK_SET_WRITER(context, _writer, _user)
 
#define MSGPACK_BUFFER_USED(ctx)   (uint16_t)((ctx)->buffer.ptr - (ctx)->buffer.buffer)
 
#define MSGPACK_BUFFER_REMAINING(ctx)   (uint16_t)((ctx)->buffer.end - (ctx)->buffer.ptr)
 
#define MSGPACK_DICT_GET_OBJECT(dict, key)   gos_msgpack_get_dict_object((const gos_msgpack_object_dict_t*)dict, key, MSGPACK_TYPE_ANY)
 
#define MSGPACK_ARRAY_GET_OBJECT(array, index)   gos_msgpack_get_array_object((gos_msgpack_object_array_t*)array, index, MSGPACK_TYPE_ANY)
 
#define MSGPACK_FOREACH(dict_or_array, callback, arg)   gos_msgpack_foreach((const gos_msgpack_object_t*)dict_or_array, callback, arg, 0)
 
#define MSGPACK_FOREACH_RECURSIVE(dict_or_array, callback, arg)   gos_msgpack_foreach((const gos_msgpack_object_t*)dict_or_array, callback, arg, UINT32_MAX)
 
#define MSGPACK_FREE_OBJECTS(obj)   gos_msgpack_free_objects(obj)
 

Detailed Description

MessagePack macros.

Macro Definition Documentation

◆ MSGPACK_ARRAY

#define MSGPACK_ARRAY (   obj,
  index 
)    gos_msgpack_get_array_object((gos_msgpack_object_array_t*)obj, index, MSGPACK_TYPE_ANY)

Get MessagePack object at specific index of array

◆ MSGPACK_ARRAY_ARRAY

#define MSGPACK_ARRAY_ARRAY (   obj,
  index 
)    (gos_msgpack_object_array_t*)MSGPACK_ARRAY_TYPE(obj, index, ARRAY)

Get MessagePack array at index with a ARRAY type, return NULL if the entry is found but the wrong type

◆ MSGPACK_ARRAY_BIN

#define MSGPACK_ARRAY_BIN (   obj,
  index 
)    (gos_msgpack_object_bin_t*)MSGPACK_ARRAY_TYPE(obj, index, BIN)

Get MessagePack array at index with a BIN type, return NULL if the entry is found but the wrong type

◆ MSGPACK_ARRAY_DICT

#define MSGPACK_ARRAY_DICT (   obj,
  index 
)    (gos_msgpack_object_dict_t*)MSGPACK_ARRAY_TYPE(obj, index, DICT)

Get MessagePack array at index with a DICT type, return NULL if the entry is found but the wrong type

◆ MSGPACK_ARRAY_GET_OBJECT

#define MSGPACK_ARRAY_GET_OBJECT (   array,
  index 
)    gos_msgpack_get_array_object((gos_msgpack_object_array_t*)array, index, MSGPACK_TYPE_ANY)

Return the object a the corresponding index in an array

See also
gos_msgpack_get_array_object() for more info
Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_ARRAY_INT

#define MSGPACK_ARRAY_INT (   obj,
  index 
)    MSGPACK_ARRAY_TYPE(obj, index, INT)

Get MessagePack array at index with a signed integer (unsigned and bool included) type, return NULL if the entry is found but the wrong type

◆ MSGPACK_ARRAY_LENGTH

#define MSGPACK_ARRAY_LENGTH (   obj)    (((gos_msgpack_object_array_t*)obj)->count)

Return the number of entries in an array

Examples:
network/http_server_stream/main.c.

◆ MSGPACK_ARRAY_STR

#define MSGPACK_ARRAY_STR (   obj,
  index 
)    (gos_msgpack_object_str_t*)MSGPACK_ARRAY_TYPE(obj, index, STR)

Get MessagePack array at index with a STR type, return NULL if the entry is found but the wrong type

Examples:
network/http_server_stream/main.c.

◆ MSGPACK_ARRAY_TYPE

#define MSGPACK_ARRAY_TYPE (   obj,
  index,
  type 
)    gos_msgpack_get_array_object((gos_msgpack_object_array_t*)obj, index, MSGPACK_TYPE_ ## type)

Get MessagePack array at index with a specific type, return NULL if the entry is found but the wrong type

◆ MSGPACK_ARRAY_UINT

#define MSGPACK_ARRAY_UINT (   obj,
  index 
)    MSGPACK_ARRAY_TYPE(obj, index, UINT)

Get MessagePack array at index with a unsigned integer (signed and bool included) type, return NULL if the entry is found but the wrong type

◆ MSGPACK_BIN

#define MSGPACK_BIN (   obj,
  mem,
  max_length 
)    memcpy(mem, MSGPACK_BIN_VALUE(obj), MIN(max_length, MSGPACK_BIN_LENGTH(obj)))

Copy BIN obj contents to buffer

Examples:
demo/secure_element/commands.c.

◆ MSGPACK_BIN_CMP

#define MSGPACK_BIN_CMP (   obj,
  mem 
)    memcmp(MSGPACK_BIN_VALUE(obj), mem, MSGPACK_BIN_LENGTH(obj))

Compare binary MessagePack object to another binary value

◆ MSGPACK_BIN_LENGTH

#define MSGPACK_BIN_LENGTH (   obj)    ((const gos_msgpack_object_bin_t*)(obj))->length

◆ MSGPACK_BIN_VALUE

#define MSGPACK_BIN_VALUE (   obj)    ((const gos_msgpack_object_bin_t*)(obj))->data

◆ MSGPACK_BOOL

#define MSGPACK_BOOL (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t, boolean)

Get MessagePack object as boolean

Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_BUFFER_REMAINING

#define MSGPACK_BUFFER_REMAINING (   ctx)    (uint16_t)((ctx)->buffer.end - (ctx)->buffer.ptr)

Return the number of data buffer bytes unused (i.e. available) by a gos_msgpack_context_t

Parameters
ctxgos_msgpack_context_t initialized with a data buffer

◆ MSGPACK_BUFFER_USED

#define MSGPACK_BUFFER_USED (   ctx)    (uint16_t)((ctx)->buffer.ptr - (ctx)->buffer.buffer)

Return the number of data buffer bytes currently used by a gos_msgpack_context_t

Parameters
ctxgos_msgpack_context_t initialized with a data buffer
Examples:
demo/secure_element/commands.c, hurricane/security_camera/camera.c, hurricane/security_camera/main.c, and utility/msgpack/read_write_buffer.c.

◆ MSGPACK_DICT

#define MSGPACK_DICT (   obj,
  key 
)    gos_msgpack_get_dict_object((gos_msgpack_object_dict_t*)obj, key, MSGPACK_TYPE_ANY)

Get MessagePack object with specific key in dictionary (aka map)

Examples:
demo/3d_demo/main.c, and demo/accelerometer_stream/main.c.

◆ MSGPACK_DICT_ARRAY

#define MSGPACK_DICT_ARRAY (   obj,
  key 
)    (gos_msgpack_object_array_t*)MSGPACK_DICT_TYPE(obj, key, ARRAY)

Get MessagePack dictionary entry with a ARRAY type, return NULL if the entry is found but the wrong type

◆ MSGPACK_DICT_BIN

#define MSGPACK_DICT_BIN (   obj,
  key 
)    (gos_msgpack_object_bin_t*)MSGPACK_DICT_TYPE(obj, key, BIN)

Get MessagePack dictionary entry with a BIN type, return NULL if the entry is found but the wrong type

Examples:
demo/secure_element/commands.c.

◆ MSGPACK_DICT_DICT

#define MSGPACK_DICT_DICT (   obj,
  key 
)    (gos_msgpack_object_dict_t*)MSGPACK_DICT_TYPE(obj, key, DICT)

Get MessagePack dictionary entry with a DICT type, return NULL if the entry is found but the wrong type

Examples:
hurricane/security_camera/camera.c, and hurricane/security_camera/main.c.

◆ MSGPACK_DICT_GET_OBJECT

#define MSGPACK_DICT_GET_OBJECT (   dict,
  key 
)    gos_msgpack_get_dict_object((const gos_msgpack_object_dict_t*)dict, key, MSGPACK_TYPE_ANY)

Return an object for the corresponding key in a dictionary

See also
gos_msgpack_get_dict_object for more info
Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_DICT_INT

#define MSGPACK_DICT_INT (   obj,
  key 
)    MSGPACK_DICT_TYPE(obj, key, INT_OR_UINT)

Get MessagePack dictionary entry with an signed integer (unsigned and bool included) type. Use MSGPACK_DICT_TYPE(obj, key, INT) if you specifically need a signed integer. return NULL if the entry is found but the wrong type

Examples:
hurricane/arducam/camera.c, and hurricane/security_camera/camera.c.

◆ MSGPACK_DICT_STR

#define MSGPACK_DICT_STR (   obj,
  key 
)    (gos_msgpack_object_str_t*)MSGPACK_DICT_TYPE(obj, key, STR)

Get MessagePack dictionary entry with a STR type, return NULL if the entry is found but the wrong type

Examples:
demo/3d_demo/main.c, demo/accelerometer_stream/main.c, demo/secure_element/commands.c, hurricane/security_camera/main.c, and network/http_server_stream/main.c.

◆ MSGPACK_DICT_TYPE

#define MSGPACK_DICT_TYPE (   obj,
  key,
  type 
)    gos_msgpack_get_dict_object((gos_msgpack_object_dict_t*)obj, key, MSGPACK_TYPE_ ## type)

Get MessagePack dictionary entry with a specific type, return NULL if the entry is found but the wrong type

◆ MSGPACK_DICT_UINT

#define MSGPACK_DICT_UINT (   obj,
  key 
)    MSGPACK_DICT_TYPE(obj, key, INT_OR_UINT)

Get MessagePack dictionary entry with a unsigned integer (signed and bool included) type, Use MSGPACK_DICT_TYPE(obj, key, UINT) if you specifically need an unsigned integer. return NULL if the entry is found but the wrong type

◆ MSGPACK_DOUBLE

#define MSGPACK_DOUBLE (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t, dbl)

Get MessagePack object as double

◆ MSGPACK_FALSE

#define MSGPACK_FALSE   0xC2

Raw value of a MessagePack FALSE boolean typed object

◆ MSGPACK_FLOAT

#define MSGPACK_FLOAT (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t, flt)

Get MessagePack object as float

◆ MSGPACK_FOREACH

#define MSGPACK_FOREACH (   dict_or_array,
  callback,
  arg 
)    gos_msgpack_foreach((const gos_msgpack_object_t*)dict_or_array, callback, arg, 0)

Non-recursively iterate the key/value pairs of a dictionary or entries in array

See also
gos_msgpack_foreach() for more info

◆ MSGPACK_FOREACH_RECURSIVE

#define MSGPACK_FOREACH_RECURSIVE (   dict_or_array,
  callback,
  arg 
)    gos_msgpack_foreach((const gos_msgpack_object_t*)dict_or_array, callback, arg, UINT32_MAX)

Recursively iterate the key/value pairs of a dictionary or entries in array

See also
gos_msgpack_foreach() for more info
Examples:
cloud/dps_demo/main.c, and dms/messages/main.c.

◆ MSGPACK_FREE_OBJECTS

#define MSGPACK_FREE_OBJECTS (   obj)    gos_msgpack_free_objects(obj)

De-allocate all objects assoicated with supplied object

See also
gos_msgpack_free_objects() for more info
Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_INIT_CONTEXT_WITH_BUFFER

#define MSGPACK_INIT_CONTEXT_WITH_BUFFER (   context,
  _buf,
  _len 
)
Value:
(context)->buffer.buffer = (uint8_t*)_buf; \
(context)->buffer.ptr = (uint8_t*)_buf; \
(context)->buffer.end = (uint8_t*)_buf + _len; \
(context)->writer = NULL; \
(context)->flags = 0; \
(context)->user = NULL

Declare and initialize a gos_msgpack_context_t with the supplied buffer

Parameters
contextPointer to gos_msgpack_context_t being initialized
_bufData buffer to initialize context with
_lenLength of supplied data buffer

◆ MSGPACK_INIT_WITH_BUFFER

#define MSGPACK_INIT_WITH_BUFFER (   name,
  _buf,
  _len 
)
Value:
{ \
.buffer.buffer = _buf, \
.buffer.ptr = _buf, \
.buffer.end = _buf + _len, \
.writer = NULL, \
.flags = 0, \
.user = NULL \
}
uint8_t * buffer
buffer to hold 'packed' message data
Definition: gos_msgpack.h:692
Definition: gos_msgpack.h:688

Declare and initialize a gos_msgpack_context_t with the supplied buffer

Parameters
nameThe variable name of gos_msgpack_context_t being declared
_bufData buffer to initialize context with
_lenLength of supplied data buffer
Examples:
demo/secure_element/commands.c, hurricane/security_camera/camera.c, hurricane/security_camera/main.c, and utility/msgpack/read_write_buffer.c.

◆ MSGPACK_INIT_WITH_WRITER

#define MSGPACK_INIT_WITH_WRITER (   name,
  _writer,
  _user 
)
Value:
{ \
.writer = _writer, \
.user = _user, \
.flags = 0, \
.buffer.buffer = NULL, \
.buffer.ptr = NULL \
}
gos_msgpack_writer_t writer
Data writer, see gos_msgpack_writer_t.
Definition: gos_msgpack.h:696
Definition: gos_msgpack.h:688

Declare and initialize a gos_msgpack_context_t with the supplied gos_msgpack_writer_t

Parameters
nameThe variable name of gos_msgpack_context_t being declared
_writerMessagePack data writer, see gos_msgpack_writer_t
_userOptional user argument given to the data writer
Examples:
system/core_dump/main.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_INT

#define MSGPACK_INT (   obj)    gos_msgpack_get_int(obj)

Get MessagePack object as a signed 32bit value

See also
gos_gos_msgpack_get_int() for more info
Examples:
hurricane/arducam/camera.c, and hurricane/security_camera/camera.c.

◆ MSGPACK_INT16

#define MSGPACK_INT16 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t, s)

Get MessagePack object as signed 16bit

See also
MSGPACK_INT() to automatically determine the integer bit size

◆ MSGPACK_INT32

#define MSGPACK_INT32 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t, s)

Get MessagePack object as signed 32bit

See also
MSGPACK_INT() to automatically determine the integer bit size

◆ MSGPACK_INT64

#define MSGPACK_INT64 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t, s)

Get MessagePack object as signed 64bit

See also
MSGPACK_LONG() to automatically determine the integer bit size

◆ MSGPACK_INT8

#define MSGPACK_INT8 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t, s)

Get MessagePack object as signed 8bit

See also
MSGPACK_INT() to automatically determine the integer bit size

◆ MSGPACK_IS_ARRAY

#define MSGPACK_IS_ARRAY (   obj)    _MSGPACK_IS_(obj, ARRAY)

Return true if MessagePack object is an array

Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_IS_BIN

#define MSGPACK_IS_BIN (   obj)    _MSGPACK_IS_(obj, BIN)

Return true if MessagePack object is a binary string

Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_IS_BOOL

#define MSGPACK_IS_BOOL (   obj)    _MSGPACK_IS_(obj, BOOL)

Return true if MessagePack object is a boolean

Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_IS_DICT

#define MSGPACK_IS_DICT (   obj)    _MSGPACK_IS_(obj, DICT)

Return true if MessagePack object is a dictionary (aka map)

Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_IS_DOUBLE

#define MSGPACK_IS_DOUBLE (   obj)    _MSGPACK_IS_(obj, DOUBLE)

Return true if MessagePack object is a double

◆ MSGPACK_IS_FLOAT

#define MSGPACK_IS_FLOAT (   obj)    _MSGPACK_IS_(obj, FLOAT)

Return true if MessagePack object is a float

◆ MSGPACK_IS_INT

#define MSGPACK_IS_INT (   obj)    gos_msgpack_object_is_type((gos_msgpack_object_t*)obj, MSGPACK_TYPE_INT)

Return true if MessagePack object is an signed integer

◆ MSGPACK_IS_INT16

#define MSGPACK_IS_INT16 (   obj)    _MSGPACK_IS_(obj, INT16)

Return true if MessagePack object is a signed 16bit integer

◆ MSGPACK_IS_INT32

#define MSGPACK_IS_INT32 (   obj)    _MSGPACK_IS_(obj, INT32)

Return true if MessagePack object is a signed 32bit integer

◆ MSGPACK_IS_INT64

#define MSGPACK_IS_INT64 (   obj)    _MSGPACK_IS_(obj, INT64)

Return true if MessagePack object is a signed 64bit integer

◆ MSGPACK_IS_INT8

#define MSGPACK_IS_INT8 (   obj)    _MSGPACK_IS_(obj, INT8)

Return true if MessagePack object is a signed 8bit integer

◆ MSGPACK_IS_NIL

#define MSGPACK_IS_NIL (   obj)    _MSGPACK_IS_(obj, NIL)

Return true if MessagePack object is a NIL (i.e. NULL value)

◆ MSGPACK_IS_STR

#define MSGPACK_IS_STR (   obj)    _MSGPACK_IS_(obj, STR)

Return true if MessagePack object is a string

Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_IS_UINT

#define MSGPACK_IS_UINT (   obj)    gos_msgpack_object_is_type((gos_msgpack_object_t*)obj, MSGPACK_TYPE_UINT)

Return true if MessagePack object is an unsigned integer

◆ MSGPACK_IS_UINT16

#define MSGPACK_IS_UINT16 (   obj)    _MSGPACK_IS_(obj, UINT16)

Return true if MessagePack object is an unsigned 16bit integer

◆ MSGPACK_IS_UINT32

#define MSGPACK_IS_UINT32 (   obj)    _MSGPACK_IS_(obj, UINT32)

Return true if MessagePack object is an unsigned 32bit integer

◆ MSGPACK_IS_UINT64

#define MSGPACK_IS_UINT64 (   obj)    _MSGPACK_IS_(obj, UINT64)

Return true if MessagePack object is an unsigned 64bit integer

◆ MSGPACK_IS_UINT8

#define MSGPACK_IS_UINT8 (   obj)    _MSGPACK_IS_(obj, UINT8)

Return true if MessagePack object is an unsigned 8bit integer

◆ MSGPACK_LONG

#define MSGPACK_LONG (   obj,
  buffer 
)    gos_msgpack_get_long(obj, buffer)

Get MessagePack object as a signed 64bit value

See also
gos_gos_msgpack_get_int() for more info

◆ MSGPACK_NIL

#define MSGPACK_NIL   0xC0

Raw value of a MessagePack NIL typed object

◆ MSGPACK_SET_WRITER

#define MSGPACK_SET_WRITER (   context,
  _writer,
  _user 
)
Value:
context->writer = _writer; \
context->user = _user; \
context->buffer.buffer = NULL; \
context->buffer.ptr = NULL

Configure the given gos_msgpack_context_t with a gos_msgpack_writer_t

Parameters
contextPointer to previously declared/allocated gos_msgpack_context_t
_writerMessagePack data writer, see gos_msgpack_writer_t
_userOptional user argument given to the data writer

◆ MSGPACK_STR

#define MSGPACK_STR (   obj,
  buffer,
  max_length 
)    gos_msgpack_get_str((gos_msgpack_object_t*)obj, buffer, max_length)

◆ MSGPACK_STR_CMP

#define MSGPACK_STR_CMP (   obj,
  str 
)    gos_msgpack_str_cmp((gos_msgpack_object_t*)obj, str)

Compare string MessagePack object to another string

◆ MSGPACK_STR_LENGTH

#define MSGPACK_STR_LENGTH (   obj)    ((const gos_msgpack_object_str_t*)(obj))->length

Get MessagePack object string length

◆ MSGPACK_STR_VALUE

#define MSGPACK_STR_VALUE (   obj)    ((const gos_msgpack_object_str_t*)(obj))->data

Get string MessagePack object's string value

Note
The string value is NOT null-terminated
See also
MSGPACK_STR()

◆ MSGPACK_TO_STR

#define MSGPACK_TO_STR (   obj,
  buffer,
  max_length 
)    gos_msgpack_to_str((gos_msgpack_object_t*)obj, buffer, max_length)

Convert an object to a string and add to buffer

Note
The buffer must be at least 32 bytes
Examples:
cloud/dps_demo/main.c, dms/messages/main.c, and hurricane/security_camera/main.c.

◆ MSGPACK_TRUE

#define MSGPACK_TRUE   0xC3

Raw value of a MessagePack TRUE boolean typed object

◆ MSGPACK_UINT

#define MSGPACK_UINT (   obj)    gos_msgpack_get_uint(obj)

Get MessagePack object as an unsigned 32bit value

See also
gos_gos_msgpack_get_int() for more info
Examples:
demo/3d_demo/main.c, demo/accelerometer_stream/main.c, utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.

◆ MSGPACK_UINT16

#define MSGPACK_UINT16 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object16_t, u)

Get MessagePack object as unsigned 16bit

See also
MSGPACK_UINT() to automatically determine the integer bit size

◆ MSGPACK_UINT32

#define MSGPACK_UINT32 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object32_t, u)

Get MessagePack object as unsigned 32bit

See also
MSGPACK_UINT() to automatically determine the integer bit size

◆ MSGPACK_UINT64

#define MSGPACK_UINT64 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object64_t, u)

Get MessagePack object as unsigned 64bit

See also
MSGPACK_ULONG() to automatically determine the integer bit size

◆ MSGPACK_UINT8

#define MSGPACK_UINT8 (   obj)    _MSGPACK_GET_OBJ_VALUE_(obj, gos_msgpack_object8_t, u)

Get MessagePack object as unsigned 8bit

See also
MSGPACK_UINT() to automatically determine the integer bit size

◆ MSGPACK_ULONG

#define MSGPACK_ULONG (   obj,
  buffer 
)    gos_msgpack_get_ulong(obj, buffer)

Get MessagePack object as an unsigned 64bit value

See also
gos_gos_msgpack_get_int() for more info
Examples:
utility/msgpack/read_write_buffer.c, and utility/msgpack/read_write_stream.c.