gos_softap_client_t Struct Reference

Contains information about a SoftAP client. More...

Data Fields

gos_mac_t mac
Mac address.
bool valid
Connection status.
uint8_t reserved
Addtional client information (specific to the softap type)
uint32_t ipv4_address
IPv4 address of client.

Detailed Description

Contains information about a SoftAP client.

Examples:
network/softap_tcp_server/main.c , and wifi/web_setup/main.c .