gos_http_upload_t Struct Reference
HTTP upload context used by gos_http_upload() More...
Data Fields | |
const char * | url |
The HTTP request URL, if no schema is included http:// is used. | |
const char * | local_filename |
Name of file on local file system. | |
const char * | remote_filename |
Name to save file as on server, optional, leave NULL to use local_filename. | |
const char * | content_type |
The HTTP 'content-type' to upload file as, optional, leave NULL for default. | |
const char * | form_name |
The HTTP 'form-data' name, optional, leave NULL for default. | |
const bool | decrypt |
gos_tls_certificates_t | certs |
For HTTPS (secure) request, the TLS cert filenames, gos_tls_certificates_t. | |
gos_interface_t | interface |
Network interface, gos_interface_t. | |
Detailed Description
HTTP upload context used by gos_http_upload()
Field Documentation
◆ decrypt
const bool gos_http_upload_t::decrypt |
If true AND the file has the GOS_FILE_FLAG_ENCRYPTED flag set THEN decrypt the file as it is uploaded to the server. If false AND the file has the GOS_FILE_FLAG_ENCRYPTED flag set THEN upload encrypted file to server.