gos_safe_circular_queue_t Struct Reference
Data Fields | |
uint8_t * | head |
Pointer to head of queue. | |
uint8_t * | tail |
Pointer to tail of queue. | |
uint8_t * | start |
Pointer to start of queue entry buffer. | |
uint8_t * | end |
Pointer to end of queue entry buffer. | |
uint16_t | count |
Number of entries in queue. | |
uint16_t | capacity |
Maximum number of entries queue can hold. | |
uint16_t | entry_size |
Size in bytes of each entry. | |
Detailed Description
Thread-safe circular queue context