gos_file_descriptor_t Struct Reference
Data Fields | |
gos_file_handle_t | handle |
Handle of file on file system. | |
uint32_t | position |
Current position in file. | |
uint32_t | size |
Size of file in bytes. | |
uint32_t | data_start_address |
Start address of file data in its first sector. | |
uint32_t | current_sector |
Current sector of file. | |
uint32_t | current_sector_position |
Position in current sector. | |
void * | user |
User provided pointer (not used by system) | |
void * | crypto_context |
Crypto context (system use only) | |
gos_file_mode_t | mode |
File I/O mode. | |
Detailed Description
File descriptor