gos_websocket_config_t Struct Reference
Websocket Client configuration. More...
Data Fields | |
const char * | host |
Websocket server URL. | |
gos_tls_certificates_t | certs |
TLS certificate filenames, gos_tls_certificates_t. | |
uint16_t | buffer_size |
Size of rx buffer in bytes. | |
gos_websocket_frame_type_t | frame_type |
gos_websocket_frame_type_t The websocket frame type | |
gos_interface_t | interface |
Network interface on which to connect to remote server. | |
gos_gpio_t | gpio |
GPIO to assert when socket has data to read, optional, set as GOS_GPIO_INVALID if not used. | |
Detailed Description
Websocket Client configuration.