gos_dms_messsage_config_t Struct Reference
DMS Message Configuration. More...
Data Fields | |
uint32_t | length |
bool | is_response |
gos_handler_t | handler |
uint32_t | timeout_ms |
Detailed Description
DMS Message Configuration.
This is used to configure an outgoing message to the DMS (sent via secure websocket)
Field Documentation
◆ handler
gos_handler_t gos_dms_messsage_config_t::handler |
Handler to be invoke when the outgoing receives a response from the DMS Leave NULL to not listen for the message's response The argument of the handler is a gos_msgpack_object_t which contains the parsed response If the response times-out, then the argument is NULL This executes in the User App Thread
◆ is_response
bool gos_dms_messsage_config_t::is_response |
Set to true if this message is a response to a received message. If this is set to true then you must manually write the message ID field to message
◆ length
uint32_t gos_dms_messsage_config_t::length |
The message's payload length. Leave a 0 if the initial length is unknown
- Note
- If the length = 0, then the entire message is buffered to RAM before transmitting to the DMS If the length > 0, then the message is transmitted to the DMS as it is written.
◆ timeout_ms
uint32_t gos_dms_messsage_config_t::timeout_ms |
Maximum in milliseconds to wait for the message's response On timeout, the supplied handler
is invoked with a NULL argument