Event data types. More...

Enumerations

enum gos_event_flag_t {
GOS_EVENT_FLAG_NONE = 0,
GOS_EVENT_FLAG_RUN_NOW = (1 << 0),
GOS_EVENT_FLAG_ALLOW_DUPLICATE = (1 << 1),
GOS_EVENT_FLAG_REQUIRE_WLAN = (1 << 3),
GOS_EVENT_FLAG_REQUIRE_SOFTAP = (1 << 4),
GOS_EVENT_FLAG_REQUIRE_ETHERNET = (1 << 5),
GOS_EVENT_FLAG_IN_EVENT_THREAD = (1 << 6),
GOS_EVENT_FLAG_IN_NETWORK_WORKER = (1 << 7),
GOS_EVENT_FLAG_UPDATE_TIMEOUT = (1 << 8)
}
Event flags. More...

Detailed Description

Event data types.

Enumeration Type Documentation

◆ gos_event_flag_t

Event flags.

Enumerator
GOS_EVENT_FLAG_NONE

No event flags set.

GOS_EVENT_FLAG_RUN_NOW

Run the event immediately (should be used with gos_event_register_periodic() )

GOS_EVENT_FLAG_ALLOW_DUPLICATE

Allow duplicate event handler.

GOS_EVENT_FLAG_REQUIRE_WLAN

The event won't execute unless the GOS_INTERFACE_WLAN interface is up.

GOS_EVENT_FLAG_REQUIRE_SOFTAP

The event won't execute unless the GOS_INTERFACE_SOFTAP interface is up.

GOS_EVENT_FLAG_REQUIRE_ETHERNET

The event won't execute unless the GOS_INTERFACE_ETHERNET interface is up.

GOS_EVENT_FLAG_IN_EVENT_THREAD

The event will execute in the system event thread (.

Note
the event MUST NOT block as no other events will execute until it completes)
GOS_EVENT_FLAG_IN_NETWORK_WORKER

The event will execute in the networking work thread.

GOS_EVENT_FLAG_UPDATE_TIMEOUT

Update a timed event's timeout if it's currently pending.