Deprecated Functions
Description
Deprecated Functions.
Data Structures |
|
| struct | SE_OTPInit_t |
|
SE OTP initialization struct.
|
|
| struct | SE_DebugStatus_t |
|
SE debug status.
|
|
| struct | SE_Status_t |
|
SE status.
|
|
Functions |
|
| SE_Response_t |
SE_initPubkey
(uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature)
|
| SE_Response_t |
SE_initOTP
(
SE_OTPInit_t
*otp_init)
|
Function Documentation
◆ SE_initPubkey()
| SE_Response_t SE_initPubkey | ( | uint32_t |
key_type,
|
| void * |
pubkey,
|
||
| uint32_t |
numBytes,
|
||
| bool |
signature
|
||
| ) |
Init pubkey or pubkey signature.
Initialize public key stored in the SE, or its corresponding signature. The command can be used to write:
- SE_KEY_TYPE_BOOT – public key used to perform secure boot
- SE_KEY_TYPE_AUTH – public key used to perform secure debug
- Note
- These keys can not be overwritten, so this command can only be issued once per key per part.
- Parameters
-
[in] key_typeID of key type to initialize. [in] pubkeyPointer to a buffer that contains the public key or signature. Must be word aligned and have a length of 64 bytes. [in] numBytesLength of pubkey buffer (64 bytes). [in] signatureIf true, initialize signature for the specified key type instead of the public key itself.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully SE_RESPONSE_TEST_FAILEDwhen the pubkey is not set SE_RESPONSE_INVALID_PARAMETERwhen an invalid type is passed
◆ SE_initOTP()
| SE_Response_t SE_initOTP | ( | SE_OTPInit_t * |
otp_init
|
) |
Initialize SE one-time-programmable (OTP) configuration.
Configuration is performed by setting the desired options in the SE_OTPInit_t structure.
This function can be used to enable secure boot, to configure flash page locking, and to enable anti-rollback protection when using the SE to perform an application upgrade, typically a Gecko bootloader upgrade.
Before secure boot can be enabled, the public key used for secure boot verification must be uploaded using
SE_initPubkey()
.
- Warning
- This command can only be executed once per device! When the configuration has been programmed it is not possible to update any of the fields.
- Parameters
-
[in] otp_initSE_OTPInit_t structure containing the SE configuration.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully