SE_Command_t Struct Reference

SE Command structure to which all commands to the SE must adhere.

#include <em_se.h>

Data Fields

uint32_t command
SE Command.
SE_DataTransfer_t * data_in
Input data.
SE_DataTransfer_t * data_out
Output data.
uint32_t parameters [ SE_MAX_PARAMETERS ]
Parameters.
size_t num_parameters
Number of parameters.

SE Command structure to which all commands to the SE must adhere.

Field Documentation

◆ command

uint32_t SE_Command_t::command

SE Command.

◆ data_in

SE_DataTransfer_t * SE_Command_t::data_in

Input data.

◆ data_out

SE_DataTransfer_t * SE_Command_t::data_out

Output data.

◆ parameters

uint32_t SE_Command_t::parameters[ SE_MAX_PARAMETERS ]

Parameters.

◆ num_parameters

size_t SE_Command_t::num_parameters

Number of parameters.