EUSART_IrDAInit_TypeDef Struct Reference

IrDA Initialization structure.

#include <em_eusart.h>

Data Fields

EUSART_UartInit_TypeDef init
General EUSART initialization structure.
bool irDALowFrequencyEnable
Enable the IrDA low frequency mode. Only Rx operation are enabled.
EUSART_IrDARxFilterEnable_TypeDef irDARxFilterEnable
Set to enable filter on IrDA demodulator.
EUSART_IrDAPulseWidth_Typedef irDAPulseWidth
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.

IrDA Initialization structure.

Field Documentation

◆ init

EUSART_UartInit_TypeDef EUSART_IrDAInit_TypeDef::init

General EUSART initialization structure.

◆ irDALowFrequencyEnable

bool EUSART_IrDAInit_TypeDef::irDALowFrequencyEnable

Enable the IrDA low frequency mode. Only Rx operation are enabled.

◆ irDARxFilterEnable

EUSART_IrDARxFilterEnable_TypeDef EUSART_IrDAInit_TypeDef::irDARxFilterEnable

Set to enable filter on IrDA demodulator.

◆ irDAPulseWidth

EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth

Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.