IADC_ScanTableEntry_t Struct Reference
IADC scan table entry structure.
#include <em_iadc.h>
Data Fields |
|
| IADC_NegInput_t | negInput |
|
Port/pin input for the negative side of the ADC.
|
|
| IADC_PosInput_t | posInput |
|
Port/pin input for the positive side of the ADC.
|
|
| uint8_t | configId |
|
Configuration id.
|
|
| bool | compare |
|
Perform digital window comparison on the result from this entry.
|
|
| bool | includeInScan |
|
Include this scan table entry in scan operation.
|
|
IADC scan table entry structure.
Field Documentation
◆ negInput
| IADC_NegInput_t IADC_ScanTableEntry_t::negInput |
Port/pin input for the negative side of the ADC.
◆ posInput
| IADC_PosInput_t IADC_ScanTableEntry_t::posInput |
Port/pin input for the positive side of the ADC.
◆ configId
| uint8_t IADC_ScanTableEntry_t::configId |
Configuration id.
◆ compare
| bool IADC_ScanTableEntry_t::compare |
Perform digital window comparison on the result from this entry.
◆ includeInScan
| bool IADC_ScanTableEntry_t::includeInScan |
Include this scan table entry in scan operation.