ECDSA signing functionality for the bootloader.
|
int32_t | btl_verifyEcdsaP256r1 (const uint8_t *sha256, const uint8_t *signatureR, const uint8_t *signatureS, const uint8_t *keyX, const uint8_t *keyY) |
|
int32_t btl_verifyEcdsaP256r1 |
( |
const uint8_t * |
sha256, |
|
|
const uint8_t * |
signatureR, |
|
|
const uint8_t * |
signatureS, |
|
|
const uint8_t * |
keyX, |
|
|
const uint8_t * |
keyY |
|
) |
| |
Verify an ECDSA signature of a SHA256-hash using secp256r1.
Verifies the authenticity of data by checking the ECDSA signature of the data's SHA256-hash. This function is only for use with the secp256r1 curve. The public key which the signature is validated against will be retrieved from the respective tokens in the lockbits-page.
- Parameters
-
sha256 | The hash of the data which is authenticated |
signatureR | Byte array (MSB first) of R-point of the ECDSA signature |
signatureS | Byte array (MSB first) of S-point of the ECDSA signature |
keyX | Pointer to the X coordinate of the ECDSA public key |
keyY | Pointer to the Y coordinate of the ECDSA public key |
- Returns
- BOOTLOADER_OK if signature is valid, else error code in BOOTLOADER_ERROR_SECURITY_BASE range.