ParserContext_t Struct ReferenceComponents > Image Parser > GBL Parser
Description
Image parser context definition.
Definition at line
197
of file
btl_gbl_parser.h
.
#include <
btl_gbl_parser.h
>
Data Fields |
|
uint8_t | internalBuffer [64] |
Buffer contents.
|
|
uint8_t | bytesInInternalBuffer |
Amount of bytes present in buffer.
|
|
uint8_t | internalBufferOffset |
Current reading offset into the buffer (circular)
|
|
uint8_t | flags |
Parser flags.
|
|
bool | inEncryptedContainer |
Parser is currently inside an encrypted tag.
|
|
bool | gotSignature |
Parser has received and verified signature.
|
|
uint8_t | receivedFlags |
Parser has received bootloader upgrade tag.
|
|
GblParserState_t | internalState |
State of the GBL parser state machine.
|
|
void * | aesContext |
AES-CCM decryption (= AES-CTR) context.
|
|
void * | shaContext |
SHA256 hashing context.
|
|
size_t | lengthOfTag |
Total length of the tag currently being parsed.
|
|
size_t | offsetInTag |
Current offset into tag being parsed.
|
|
size_t | lengthOfEncryptedTag |
Total length of current encrypted data block.
|
|
size_t | offsetInEncryptedTag |
Offset into current encrypted data block.
|
|
uint32_t | programmingAddress |
Current address the image needs to be written to.
|
|
uint32_t | tagAddress |
Current offset of metadata/bootloader being handled (starts at 0)
|
|
uint8_t | withheldApplicationVectors [24] |
Withheld application data.
|
|
uint8_t | withheldUpgradeVectors [4] |
Withheld bootloader upgrade data during app parsing.
|
|
uint8_t | withheldBootloaderVectors [4] |
Withheld bootloader upgrade data during bootloader parsing.
|
|
uint32_t | fileCrc |
Running CRC-32 over the incoming GBL file.
|
|
uint32_t | customTagId |
Context for custom tag.
|
|
The documentation for this struct was generated from the following file:
-
btl_gbl_parser.h