BootloadInfo_t Struct ReferenceComponents > Storage > Bootload Info
Description
Definition of the Bootload Info struct.
The Bootload Info struct contains a prioritized list of firmware update images that the bootloader should attempt to bootload. The first image to pass verification will be bootloaded.
Definition at line 65
of file btl_storage_bootloadinfo.h
.
#include <
btl_storage_bootloadinfo.h
>
Data Fields | |
uint32_t | magic |
Magic word indicating that this is a Bootload Info struct (BTL_STORAGE_BOOTLOADINFO_MAGIC) | |
uint32_t | structVersion |
Struct version number. | |
uint32_t | length |
Size of the BootloadInfo_t struct. | |
int32_t | bootloadList [BTL_STORAGE_BOOTLOAD_LIST_MAX_LENGTH] |
List of addresses of slots to bootload from. | |
uint32_t | crc32 |
Checksum of the struct. | |
The documentation for this struct was generated from the following file:
btl_storage_bootloadinfo.h