GblEncryptionData_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format
Description
GBL encryption data tag type.
Definition at line 212
of file btl_gbl_format.h
.
#include <
btl_gbl_format.h
>
Data Fields | |
GblTagHeader_t | header |
Tag ID and length. | |
uint8_t * | encryptedGblData |
Encrypted data. | |
Field Documentation
uint8_t* GblEncryptionData_t::encryptedGblData |
Encrypted data.
After decryption, this data must represent one or more complete unencrypted GBL tags.
Definition at line 214
of file btl_gbl_format.h
.
The documentation for this struct was generated from the following file:
btl_gbl_format.h