GblTagHeader_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format

Description

GBL tag header. Must be the first element in all GBL tags.

Definition at line 142 of file btl_gbl_format.h .

#include < btl_gbl_format.h >

Data Fields

uint32_t tagId
Tag ID.
uint32_t length
Length (in bytes) of the rest of the tag.

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h