BootloaderParserCallbacks_t Struct ReferenceApplication Interface > Application Parser Interface

Description

Function pointers to parser callbacks.

Definition at line 57 of file btl_interface_parser.h .

#include < btl_interface_parser.h >

Data Fields

void * context
Opaque pointer passed to the callback functions.
BootloaderParserCallback_t applicationCallback
Callback function pointer for application image data.
BootloaderParserCallback_t metadataCallback
Callback function pointer for image metadata.
BootloaderParserCallback_t bootloaderCallback
Callback function pointer for bootloader upgrade image data.

The documentation for this struct was generated from the following file:
  • btl_interface_parser.h