BareBootTable_t Struct ReferenceApplication Interface > Common Application Interface
Description
Bare boot table. Can be mapped on top of vector table to access contents.
Definition at line 57
of file btl_interface.h
.
#include <
btl_interface.h
>
Data Fields | |
uint32_t * | stackTop |
Pointer to top of stack. | |
void(* | resetVector )(void) |
Pointer to reset vector. | |
uint32_t | reserved0 [5] |
Reserved pointers to fault handlers. | |
uint32_t | reserved1 [3] |
Reserved pointers to RESERVED fields. | |
void * | table |
Pointer to bootloader table. | |
uint32_t | reserved2 [2] |
Reserved pointers to SVC and DebugMon interrupts. | |
void * | signature |
Pointer to application signature. | |
The documentation for this struct was generated from the following file:
btl_interface.h